May 14, 2026
About This Video
Battery life measured in years rather than months sets a high bar for any connected IoT device — and this webinar examines how the Renesas DA16200 Wi-Fi SoC clears it. Through its ultra-low power operation and minimal sleep currents, the DA16200 enables IoT applications to stay connected to a Wi-Fi network while running for years on standard AA batteries. The session walks through the power architecture that makes this possible, demonstrates the tools and evaluation kits available to measure and verify that performance, and highlights the DA16200's standalone capability — including the ability to run the application directly on the device itself.