Skip to main content
Renesas Electronics Corporation

Motor Workbench (Analyzer): Parameter Output Function Tutorial

Motor Workbench (Analyzer): Parameter Output Function Tutorial
May 29, 2023

About This Video

New function in RMW3.1

Output the adjusted control parameters as a header file and easily reflect them in the program

  • Output adjusted variables to header file as macro definitions
  • Select a variable to be linked to a macro definition
  • A new macro name can be added to the end of the file for output