Skip to main content
Renesas Electronics Corporation

ELCL Slave Select Pin Function (4-wire SPI) Tutorial (3/3) - Add user code and run project for RL78/G23

ELCL Slave Select Pin Function (4-wire SPI) Tutorial (3/3) - Add user code and run project for RL78/G23
Jun 29, 2022

About This Video

This video demonstrates how to use e² studio to enable RL78 Logic and Event Link Controller (ELCL) function to add Slave Selection (SS) to the slave receive mode of a Serial Array Unit's (SAU) 3-wire serial I/O (CSI) and achieve 4-wire SPI (Serial Peripheral Interface) communication.