Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community
This Software / Tool Has Been Discontinued

Please contact technical support with any questions.

Description

This assembler package includes the SRA74 assembler. The powerful optimizations offer the ultimate in execution speed and code efficiency, and the utilities increase productivity.

Features

  • Structured instructions
  • Versatile macro instructions
  • Automatically selects memory-efficient addressing modes
  • Tag files generation
  • Library function
  • Free software including an absolute address list generation tool, multiple file cross referencer and others
  • Learn More

Release Information

Latest Ver.: V.4.10 Release 02

Released: Oct 1, 2005

Details of upgrade (See Tool News)

Operating Environment

Standard life cycle of Compilers (PDF | English, 日本語)

Note: Future functional extension or problem fixes are not planned.

Target Devices

Type Title Date
Upgrade - IDE
Log in to Download ZIP 14.57 MB 日本語
Upgrade - IDE
Log in to Download ZIP 66.81 MB 日本語
Upgrade - Compiler
Log in to Download EXE 52.46 MB 日本語
Upgrade - Debugger
Log in to Download EXE 5.08 MB 日本語
Upgrade - IDE
Log in to Download EXE 4.15 MB 日本語
5 items
Type Title Date
Release Note PDF 307 KB 日本語
Manual - Development Tools PDF 4.16 MB 日本語
Manual - Development Tools PDF 1.85 MB 日本語
Release Note PDF 132 KB 日本語
Release Note PDF 215 KB 日本語
Tool News - Note PDF 194 KB 日本語
Tool News - Release PDF 196 KB 日本語
Tool News - Notification PDF 195 KB 日本語
Tool News - Note PDF 194 KB 日本語
Tool News - Release PDF 194 KB 日本語
Manual - Development Tools PDF 517 KB 日本語
11 items

Functions (SRA74 Assembler)

Structured instructions

Supports C language-like assignment statements and control statements (e.g. if, for). These structured instructions clarify program's control structure and improve productivity and maintainability.

  • Bit symbol: By using structured instructions, a memory bit and accumulator bit can be referenced and modified.

    Example of modifying accumulator bit in a assignment statement:
     BIT_A0 = 0
    Example of referencing a accumulator bit in a IF statement:
     if BIT_A0
    

    The memory bit is defined as a bit symbol. The accumulator bit has reserved words.

  • Accessing directly to the internal register: By using structured instructions, the internal register and flag can be referenced and modified.

    Example of modifying the internal register in a assignment statement:
     C = 1
    Example of referencing the internal register in a IF statement:
     if C == 0
    

    The internal register and flag have reserved words.

Versatile macro instructions

Frequent instructions are defined as macro instructions to clarify programs. SRA74 supports system macro instructions and user-definable macro instructions.

Tag files generation

SRA74 generates tag files storing assembling error information. With the tag files, source files can be efficiently modified.

Library function

LIB74 librarian generates a library of versatile subroutines, which improves the diversion rate of programs.

Absolute address lists

LST74 generates an absolute address list file from relative address list files to aid in understanding overall program organization.

Cross reference lists

SRA74 generates 2 kinds of cross-referencers which generate lists of definitions and references of labels and symbols. One cross-referencer is CRF74 which generates cross reference lists in each source file, and the other is XREF74 which generates a cross reference list in more than two source files. These lists help check dependencies of labels and symbols during debugging.

Branch instruction optimizing

The LOOP74 converts from a branch instruction which causes the assembler error because of the branch address outside the legal range to the instruction that can branch without problems. With LOOP74, you can create a program including best branch instructions from one using shortest branch instructions.

Product Components

  • Relocatable assembler: sra74
  • Linker: link74
  • Librarian: lib74
  • Cross referencer: crf74
  • File converter for M37280: cv74
  • Branch optimization tool: loop74
  • Machine language file converter: hextos2
  • Multiplication & division sub-routine: sra74.a74
  • Absolute address list generation tool: lst74 (Note1)
  • Cross referencer for multiple files: xref74 (Note1)
  • PDF manual
  • Help file
  • Simulator debugger: Provides source level debugging capability in targetless system-level.
  • IDE (Integrated development environment): High-performance Embedded Workshop and TM: Provides seamless integration and easy access to all tools for coding, compiling, linking, and debugging. It greatly increases productivity.

Note

  1. These are free software, therefore the provisions of the license are not applied.

Processing Flow

Image
sra74-1