Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

Topics

  • The PG-FP6 supports the new device RX14T.

The PG-FP6 installed in a system is a tool for erasing, programming, and verifying programs on Renesas MCUs with on-chip flash memory.

Features

  • Control panel suitable for stand-alone operation [Learn More]
  • Simple and user-friendly GUI, FP6 Terminal [Learn More]
  • Useful functions for production line: programming using by buttons and automatic programming
  • Able to use USB power: convenient for programming in the field
  • High-speed programming of MCUs by the PG-FP6 for reduced production times [Learn More]
  • Support for high-volume programming by gang programming with the use of multiple PG-PF6s [Learn More]
  • Security Enhancement against theft of program files and the PG-FP6 main unit [Learn More]
  • Security slot for theft prevention
  • High-speed downloading of files for programming from a PC to the PG-FP6 [Learn More]
  • Code storage capacity with 256MB for large flash memory
  • High compatibility with the predecessor [Learn More]

Release Information

Programming GUI (FP6 Terminal)

Latest Ver. : V1.20.00 
Released : Apr. 20, 2026 
Note: The FP6 Terminal includes parameter files, firmware, and USB drivers. 
Release information (See Tool News
Operating Environment

FAQ

Title
MCU Flash Erasure at Connection with Flash Programming Tool (PG-FP5/PG-FP6/RFP/FDT)
Several MCUs "Read (R)" command is grayed and cannot be selected.
Writing to an MCU with a different ROM/RAM size (RFP/PG-FP5/PG-FP6)

See all related FAQs

See also Error Guide.

See Error Guide

Target Devices

Target Family

Note:

  1. Use programmers produced by partners for programming of the V850 and 78K with dual power supply flash memory, which assume mass production with mask ROM.
  2. For details of support for individual device part numbers, see List of MCUs supported by PG-FP6 (PDF | English, 日本語).

Downloads

Documentation

Design & Development

Product Options

Applied Filters:

Explore

Videos & Training

Additional Details

 

Control panel suitable for stand-alone operation

Image
pgfp6-contorolpanel-e

 

User-friendly GUI (FP6 Terminal)

Image
pgfp6-gui-e

 

Security Enhancement against theft of program files and the PG-FP6 main unit

The following three features are added to enhance security against theft of program files and the PG-FP6 main unit.

  • Encryption of program files
  • Saving of encrypted files in the PG-FP6 main unit
  • Simultaneous decryption and writing in the PG-FP6

The program file encryption function can be run by using the encryption utility program (RPE.exe) from the command line. The file is among those installed by the FP6 Terminal installer.

Image
pgfp6-key-en

Major Functions

  • Stand-alone programming
  • PC-controlled programming using dedicated GUI (FP6 Terminal)
  • Up to 8 savable programming environments
  • Optimized for production line programming (command control or remote control)
  • Programming a unique code to a designated area of flash memory
  • Function to control PG-FP6 main unit (prohibiting uploading and setup)
  • Encryption of program files
  • Saving of encrypted files in the PG-FP6 main unit
  • Simultaneous decryption and writing in the PG-FP6
  • Simultaneous selection of multiple program files
  • Gang programming

 

High Compatibility with the Predecessor

Designed with compatibility with the predecessor PG-FP5 in mind for smooth migration.

  • Setup files created with the PG-FP5 can be imported
  • Support of PG-FP5-enabled MCUs
    (For the V850 and 78K family, only MCUs with single-power-supply flash memory is supported.)
  • The same specifications of control buttons, message display, and status LEDs
  • The same specification of connector layout
  • Connectable to boards designed by using the PG-FP5
  • Pursuing programming GUI compatibility

*Function and performance comparisons with the PG-FP5 (Learn More >>)

Specifications

ItemDescription
Operating power supply
  • Supplied via the power adapter (5 V, 2 A): recommended
  • USB-bus power supply (VBUS 4.5 V min./500 mA max.)
Operating environment conditionTemperature: 5C to 35C (no condensation)
Storage environment conditionTemperature: 15C to 55C (no condensation)
Package size140 x 95 x 30 mm (not including projections)
WeightApproximately 245 g
Host PC interfaceTarget host PC: Refer to section 1.5, Operating Environments.
USB connector: USB 2.0 (mini-B type)
Serial port: 9-pin D-Sub male port for RS-232C Note1
Target interface15-pin D-Sub female target connector
Power supply: 1.8 V to 5.5 V, 500 mA max. Note2
Remote interface15-pin D-Sub female remote connector
Interface level: 3.3 V
Operation of the PG-FP6 main unit
  • Use of the GUI (FP6 Terminal)
  • Use of the gang programming GUI (FP6 Gang Programmer)
  • Use of communications commands
  • Standalone operation with the use of the buttons of the PG-FP6 main unit
  • Remote interface operation using signals from an external control unit
Selectable programming environmentUp to eight target environments are selectable for the programming area
(384 MB max)
Security functions of the PG-FP6 main unit
  • Pattern authentication when the main unit is started
  • Password authentication when the settings of the security function are changed
  • A limit on the number of times authentication can be attempted
  • Reading of RPE files
  • Restricting the operation of the PG-FP6 main unit (in terms of the number of times the target device can be programmed and restriction of the execution of commands)
  • Encrypting the data stored in the PG-FP6 main unit
Power adapterPower adapter for each region Note3
USB cableApproximately 2 m
Target cable14-pin type:Cable length: Approximately 42 cm
GND cableApproximately 1 m
Compliance with overseas standardsEuropean Standards: EN 55032 Class A, EN 55024
US FCC Standard: FCC part 15 Class A

Notes:

  1. Connecting to the host PC has to use a cross cable.
  2. The maximum power-supply current is 100 mA when USB bus power is being supplied; however, this depends on the performance of the USB host in terms of the supply of power.
  3. The power adapter that comes with the PG-FP6 varies with the region where it is to be used. For the product type names, see Ordering Information.

Components

PG-FP6GND cableUSB cableTarget cable (14-pin)Power supply adapter
Image
PG-FP6
Image
pgfp6_GNDcable
Image
pgfp6_USBcable
Image
pgfp6_targetcable
Image
電源 アダプタ

Notes:

  1. The regulations with which the PG-FP6 conforms and plug shape vary depending on regions where the order is made.  See Power supply adapter. >>
  2. Conversion Adapters or Cables are provided as optional products.  See optional products. >>
  3. Programming GUI, FP6 Terminal, is available here for download.

 

Ordering Information

RegionOrdering Number
JapanRTE0T00001FWRJP000R
Europe, USA  RTE0T00001FWREA000R
China, Hong Kong, Chinese Taipei, South Korea, SingaporeRTE0T00001FWRAS000R

Notes:

  1. Since regulations that apply to the PG-FP6 vary with the region, we cannot ship a product to a region other than that from which the order was made. For example, if you place an order in Japan, you cannot purchase a product intended for Europe and the USA. Please purchase the product from a Renesas Electronics Corporation representative (responsible for sales) or distributor in the region where it is to be used.
  2. If you wish to know which model is available in a region not included in the above table, please contact either a Renesas Electronics Corporation representative (responsible for sales) or distributor.
  3. The power adapter that comes with the PG-FP6 complies with the regulations that are applicable in the target region. Its plug is also in the shape that is usable in that region.

 

Power Supply Adapter

The PG-FP6 includes a power supply adapter which conforms with the regulations and plug shapes in the region where the order is made.

RegionPlug ShapeVoltage
Japan
Image
plug-a

A

AC: 100-240V Note1
Europe
Image
plug-se

SE

Image
plug-c

C

Image
plug-bf

BF

Image
plug-a

A

USA
China
Hong Kong
Chinese Taipei
South Korea
Singapore

Note:

  1. This is the range of voltages that the power-supply adapter can support. For the actual voltage through the power-supply cable, check the indication often be at the end of the casing for the plug.

PG-FP6 Usage Examples

Stand-alone (off-line) programming

Image
pgfp6_connections_standalone-en

Field programming

Image
pgfp6_field_programming-en

Production line programming

Image
pgfp6_connections_productline-en

PC programming

Image
pgfp6_connections_pc-en

Optional Products

Following optional products are provided to facilitate the use of the PG-FP6.

  • Conversion Adapter
    • 20-Pin Conversion Adapter for the PG-FP6 [RTE0T00001FWRB0000R]
    • 14-Pin to 16-Pin Conversion Adapter for the E1 Emulator  [QB-F14T16-01]
  • Converter Cable
    • User-system Interface Cable for the E2 Emulator (20-10 pins) [RTE0T00020KCAC1000J]
  • Cable
    • User-system Interface Cable for the E2 Emulator (20-20pins) [RTE0T00020KCAC0000J]

Conversion Adapter

20-Pin Conversion Adapter for the PG-FP6 [RTE0T00001FWRB0000R]

This adapter is used for converting the 15-pin D-sub connectorNote1 to be connectable to the 20-pin CoreSight connector. The adapter comes with a 20-pin CoreSight cable (approximately 150-mm long).

Purpose: Programming RA- or RE-family MCUs on boards which have 20-pin CoreSight connectors.

Note:

  1. The target connecter on the PG-FP6.
Image
20pin-adapter-pgfp6

20-Pin Conversion Adapter for the PG-FP6

14-Pin to 16-Pin Conversion Adapter for the E1 Emulator  [QB-F14T16-01]

QB-F14T16-01 ユーザーズマニュアル(E1エミュレータ用14ピン/16ピン変換アダプタ) / QB-F14T16-01 User's Manual (14-Pin to 16-Pin Conversion Adapter for E1 Emulator) (PDF)

This adapter converts the 14-pin, 2.54-mm pitch connector of the target cable to be connectable to the 16-pin, 2.54-mm pitch connector of the PG-FP5 or MINICUBE2.

Purpose: Programming 78K- or V850-family MCUs on boards which have 16-pin connectors.

Image
14 to16 adapter for E1 Eumulator
14-Pin to 16-Pin Conversion Adapter for the E1 Emulator

Converter Cable

User-system Interface Cable for the E2 Emulator (20-10 pins) [RTE0T00020KCAC1000J]

RTE0T00020KCAC1000J User's Manual User-system Interface Cable for the Emulator(20-10 pins) (PDF | English, 日本語)

This cable is used for converting a CoreSight 20-pin connector to fit a CoreSight 10-pin connector, and is available for separate purchase. Use this conversion cable (approximately 150-mm long) along with the 20-pin conversion adapter for the PG-FP6.

Purpose: Programming RA- or RE-family MCUs on boards which have 10-pin CoreSight connectors.

Image
User Interface Cable for E2 Emulator
User-system Interface Cable for the E2 Emulator (20-10 pins)

Cable

User-system Interface Cable for the E2 Emulator (20-20pins) [RTE0T00020KCAC0000J]

RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)

This 20-pin CoreSight cable (approximately 150-mm long) is available for separate purchase. This cable also comes with the 20-pin conversion adapter for the PG-FP6.

Purpose: For use when, for example, the cable that comes with the product is damaged.

Image
User Interface Cable for E2 Emulator
User-system Interface Cable for the E2 Emulator (20-20pins)
 

Support

Support Communities

  1. PG-FP6 flashing problem with RL78/G13

    I've just detected a strange problem using two PG-FP6's programmers flashing RL78/G13 uC's. They have been used for flashing this kind of uC's for some time without problems. Suddenly, when using FP6 Terminal, an error arise when flashing:   >ver Firmware Version V1.01 ...

    Aug 31, 2020
  2. Connect sh72531d with pg-fp6

    I need help connecting between SH72531D and PG-FP6. In pg-fp6 only sh72531 is available and when I use the sh72531D part the programmer receives error message 021. Thanks for help

    Jan 25, 2021
  3. R7F124FLJ - Not able to erase last block of data flash with PG-FP6

    Hi!I have an R7F124FLJ4AFB and I tried to use Security ID authentification.Thus, I wrote 16 bytes 0xAA into the code flash @ 0xD6..0xE5.After that with 0xFF I could not get in. Then I changed to 0xAA and it let me in again.So far so good. But ...

    May 9, 2024
View All Results from Support Communities (95)

Knowledge Base

  1. Programming Security IDs (PG-FP6, RH850 Family)

    ... dialog box [Flash Options] tabbed page. Select [Security Code] and [Set].② Open the [Operation Settings] tabbed page, and then check the [Program Flash Options] checkbox.③ Execute any of the following. [Program Flash Options] in the [Target] menu Communications command pfo [Set Option] in the PG-FP6 display menu

    Mar 29, 2022
  2. Settings Used When Measuring Programming Speeds of PG-FP5 and PG-FP6

    ... PG-FP5: 2 Mbps (MAX)PG-FP6: 2.5 Mbps (MAX)   Note that the fastest programming method for RH850/E1M-S2 (320 MHz) to use CSI 5 Mbps. For your reference, programming speed is 16 seconds. Programming speed of CSI is the same with PG-FP5 and PG-FP6.

    Jan 28, 2019
  3. Remote interface control (PG-FP5/PG-FP6)

    ... /PG-FP6 successively performs the commands specified in the downloaded setting file.If you want to use the remote interface to perform erase, program, and verify operations, download the setting file (with the applicable items enabled) to the PG-FP5/PG-FP6, and then control the START signal.

    Jun 16, 2020
View All Results from Knowledge Base (139)