Skip to main content
Renesas Electronics Corporation

Overview

The EK-RA4M3 evaluation kit enables users to effortlessly evaluate the features of the RA4M3 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2 studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life.

Getting Started

Running the Quick Start Example Project

  1. The EK-RA4M3 board comes pre-programmed with a quick start example project (source code provided in the EK-RA4M3 example project bundle).
  2. Power up the EK-RA4M3 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
  3. The quick start example project will begin to execute blinking the blue user LED.
  4. Refer to the EK-RA4M3 Quick Start Guide to explore additional functionality of the quick start example project.

Developing Embedded Applications

  1. Modifying the quick start example project – refer to the EK-RA4M3 Quick Start Guide for instructions on importing, modifying, and building the quick start example project.
  2. Start with one of the many other example projects (provided in the EK-RA4M3 example project's bundle) – choose from many example projects to learn about different peripherals of the RA4M3 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.

Building Custom Hardware

  1. Start by building a functional prototype - utilize the EK-RA4M3 board with your choice of ecosystem add-ons.
  2. Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA4M3 design package.

Features

  • Special Feature Access
    • 32MB external Quad-SPI Flash
  • MCU Native Pin Access
    • R7FA4M3AF3CFB MCU
    • 100MHz, Arm Cortex®-M33 core
    • 1MB Code Flash, 128KB SRAM
    • 144 pins, LQFP package, 20mm x 20mm x 1.70mm, 0.5mm pitch
    • Native pin access through prototype friendly male headers
    • MCU and USB current measurement points
  • Ecosystem & System Control Access
    • USB full speed host and device
    • Multiple 5V input sources
      • USB (debug, full speed)
      • External power supply
    • SEGGER J-LinkTM on-board programmer and debugger
    • Debug modes
    • User LEDs and buttons
      • Three user LEDs (red, blue, green)
      • Power LED (white) indicating availability of regulated power
      • Debug LED (yellow) indicating the debug connection
      • Two user buttons
      • One reset button
    • Five most popular ecosystem expansions
      • MikroElektronika™ mikroBUS connector
      • SparkFun® Qwiic® connector
      • Two SeeedGrove® system (I2C and analog) connectors
      • Two Digilent Pmod™ (SPI and UART) connectors
      • Arduino™ (UNO R3) connector
    • MCU boot configuration

Products in the Design

Getting Started

Explore Ready-to-Run Solutions

Renesas 365 is a cloud-based platform for model-driven embedded system design that simplifies early-stage exploration and scales with your evolving needs.
Start with examples validated by Renesas engineering experts.
Launch Renesas 365

Sample & Buy

EK-RA4M3 Evaluation Board

Evaluation Kit for RA4M3 MCU Group

RTK7EKA4M3S00001BE Active
Description:Evaluation Kit for RA4M3 MCU Group
HTS (US):8471.50.0150
ECCN (US):3A991.a.2
SPQ:1
Pb (Lead) Free:No
Assembly Location:UNITED KINGDOM

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

Evaluation Kit for RA4M1 MCU Group

EK-RA4M1 Active
Enables evaluation of the RA4M1 MCU for embedded system development. Supports rapid prototyping with Renesas software tools.

Evaluation Kit for RA4M2 MCU Group

EK-RA4M2 Active
Evaluate the RA4M2 MCU using a versatile development platform with rich peripheral support. Designed to accelerate prototyping and custom hardware development.

Videos & Training

Support

Support Communities

  1. RFP doesn't work correctly in serial mode with EK-RA4M3

    Hi all, I've played a little with RFP v3.14 with my eval board EK-RA4M3.  I wanted to check some communication over UART (by using J-Link on eval board).  With baudrate 9600 everything is fine, I can read memory option bytes etc., but when I change to ...

    Feb 10, 2024
  2. EK-RA4M3 Evaluation Kit and Hello World ram overflow

    Hello I am using e2 studio and the EK-RA4M3 evaluation kit, which uses the R7FA4M3AF3CFB MCU. I followed the quick start guide, and is ready to compile the quickstart_ek_ra4m3_ep project. But whenever i compile i get this: c:/renesas/ra/e2studio_v2021-10 ...

    Dec 4, 2021
  3. Adding FreeRTOS+CLI to EK-RA4M3

    How would I go about adding FreeRTOS+CLI to my EK-RA4M3 project in E2 Studio? It is not listed as an available component. I don't want to add it directly to my source folder and have to maintain versions with FSP. Board:  EK-RA4M3Device:   R7FA4M3AF3CFB Toolchain:   GCC ...

    Nov 14, 2023
View All Results from Support Communities (50)

Knowledge Base

  1. RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)

    Last Updated: 12/14/2023 Question: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit) Answer: Renesas has equipped each EK (Evaluation Kit) for RA MCUs, such as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3 ...

    Dec 14, 2023
  2. RA Family: 16-Bit boundary byte swap in Macronix OSPI Memory DTR (DDR) Mode

    ... MX25LM51245G (OSPI)(EK-RA6M4, EK-RA6M5) 0x12345678 N/A N/A 0x12345678 0x34127856 MX25L25645G (QSPI)(EK-RA6M3, EK-RA6M4, EK-RA6M5, EK-RA4M2, EK-RA4M3) 0x12345678 0x12345678 0x12345678 N/A N/A MX25LW51245G (OSPI)(EK-RA8P1) 0x12345678 N/A N/A N/A ...

    Sep 5, 2025