Skip to main content
Renesas Electronics Corporation

Overview

The EK-RA4M2 evaluation kit enables users to effortlessly evaluate the features of the RA4M2 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2 studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life.

Getting Started

Running the Quick Start Example Project

  1. The EK-RA4M2 board comes pre-programmed with a quick start example project (source code provided in the EK-RA4M2 example project bundle).
  2. Power up the EK-RA4M2 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
  3. The quick start example project will begin to execute blinking the blue user LED.
  4. Refer to the EK-RA4M2 Quick Start Guide to explore additional functionality of the quick start example project.

Developing Embedded Applications

  1. Modifying the quick start example project – refer to the EK-RA4M2 Quick Start Guide for instructions on importing, modifying, and building the quick start example project.
  2. Start with one of the many other example projects (provided in the EK-RA4M2 example project's bundle) – choose from many example projects to learn about different peripherals of the RA4M2 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.

Building Custom Hardware

  1. Start by building a functional prototype - utilize the EK-RA4M2 board with your choice of ecosystem add-ons.
  2. Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA4M2 design package.

Features

  • Special Feature Access
    • 32MB external Quad-SPI Flash
  • MCU Native Pin Access
    • R7FA4M2AD3CFP MCU
    • 100MHz, Arm Cortex®-M33 core
    • 512KB Code Flash, 128KB SRAM
    • 100 pins, LQFP package, 14mm x 14mm x 1.70mm, 0.5mm pitch
    • Native pin access through prototype friendly male headers
    • MCU and USB current measurement points
  • Ecosystem & System Control Access
    • USB full speed host and device
    • Multiple 5V input sources
      • USB (debug, full speed)
      • External power supply
    • SEGGER J-LinkTM on-board programmer and debugger
    • Debug modes
    • User LEDs and buttons
      • Three user LEDs (red, blue, green)
      • Power LED (white) indicating availability of regulated power
      • Debug LED (yellow) indicating the debug connection
      • Two user buttons
      • One reset button
    • Five most popular ecosystem expansions
      • MikroElektronika™ mikroBUS connector
      • SparkFun® Qwiic® connector
      • Two SeeedGrove® system (I2C and analog) connectors
      • Two Digilent Pmod™ (SPI and UART) connectors
      • Arduino™ (Uno R3) connector
    • MCU boot configuration

Products in the Design

Getting Started

Explore Ready-to-Run Solutions

Renesas 365 is a cloud-based platform for model-driven embedded system design that simplifies early-stage exploration and scales with your evolving needs.
Start with examples validated by Renesas engineering experts.
Launch Renesas 365

Sample & Buy

EK-RA4M2 Evaluation Board

Evaluation Kit for RA4M2 MCU Group

RTK7EKA4M2S00001BE Active
Description:Evaluation Kit for RA4M2 MCU Group
HTS (US):8471.50.0150
ECCN (US):3A991.a.2
SPQ:1
Pb (Lead) Free:No
Assembly Location:UNITED KINGDOM

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

Evaluation Kit for RA4M1 MCU Group

EK-RA4M1 Active
Enables evaluation of the RA4M1 MCU for embedded system development. Supports rapid prototyping with Renesas software tools.

Evaluation Kit for RA4M3 MCU Group

EK-RA4M3 Active
Evaluate the RA4M3 MCU using a feature‑rich development kit with integrated debugging. Ideal for rapid prototyping and peripheral exploration.

Videos & Training

Support

Support Communities

  1. I-003 Introduction to FSP FreeRTOS Course Materials FSP 450 EK-RA4M2

    Materials for I-003 Intro to FreeRTOS Course for FSP 450 and EK-RA4M2

  2. EK-RA4M2 debug out mode doesn't work with custom board RA6M5

    Hi everyone, I try to use EK-RA4M2 debug out mode for debugging chip R7FA6M5AH3CFC on my PCB. But it doesn't work. The e2 studio report a issue that CPU_REG_SET(): Register 0 is already marked as valid. What does it mean? Does EK-RA4M2 debug out mode ...

    Jul 8, 2024
  3. From evaluation board EK-RA4M2 (with R7FA4M2AD3CFP) to a custom board with the same microcontroller...

    Hi people, as you can guess from the subject of this post I faced some problems with the custom board even with a minimal application (led blinking). I can program successfully the custon board using a USB-serial FTDI232 converter. The relevant pins of FTDI converter are conneted with the ...

    Aug 12, 2021
View All Results from Support Communities (101)

Knowledge Base

  1. RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)

    Last Updated: 12/14/2023 Question: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit) Answer: Renesas has equipped each EK (Evaluation Kit) for RA MCUs, such as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3 ...

    Dec 14, 2023
  2. RA and FSP Curriculum: I-003 Introduction to FSP FreeRTOS Lab

    ... Introduction to FSP FreeRTOS- an overview presentation covering the key features of FreeRTOS and a hands-on lab using FSP and the EK-RA6M4 or EK-RA4M2 kit. The lab illustrates the FSP implementation of key RTOS elements such as: threads/tasks, priorities,  task handles, task properties, message queues ...

    Aug 9, 2023
  3. ICODE SLIX2 Commands

    ... 2 This example contains only 3 commands (Get Random Number, Set Password and Protect Page) and the project uses the SDK's RA4M2 reference implementation (EK-RA4M2 Evaluation Board). This approach involves no changes to core SDK functions or structures. The example application executes the commands in order once a ...

    Oct 1, 2025