Overview
Description
The EK-RA4M2 evaluation kit enables users to effortlessly evaluate the features of the RA4M2 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2 studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life.
Getting Started
Running the Quick Start Example Project
- The EK-RA4M2 board comes pre-programmed with a quick start example project (source code provided in the EK-RA4M2 example project bundle).
- Power up the EK-RA4M2 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
- The quick start example project will begin to execute blinking the blue user LED.
- Refer to the EK-RA4M2 Quick Start Guide to explore additional functionality of the quick start example project.
Developing Embedded Applications
- Modifying the quick start example project – refer to the EK-RA4M2 Quick Start Guide for instructions on importing, modifying, and building the quick start example project.
- Start with one of the many other example projects (provided in the EK-RA4M2 example project's bundle) – choose from many example projects to learn about different peripherals of the RA4M2 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.
Building Custom Hardware
- Start by building a functional prototype - utilize the EK-RA4M2 board with your choice of ecosystem add-ons.
- Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA4M2 design package.
Features
- Special Feature Access
- 32MB external Quad-SPI Flash
- MCU Native Pin Access
- R7FA4M2AD3CFP MCU
- 100MHz, Arm Cortex®-M33 core
- 512KB Code Flash, 128KB SRAM
- 100 pins, LQFP package, 14mm x 14mm x 1.70mm, 0.5mm pitch
- Native pin access through prototype friendly male headers
- MCU and USB current measurement points
- Ecosystem & System Control Access
- USB full speed host and device
- Multiple 5V input sources
- USB (debug, full speed)
- External power supply
- SEGGER J-LinkTM on-board programmer and debugger
- Debug modes
- Debug on-board (SWD) – via J-Link
- Debug out (SWD) – via J-Link
- Debug in (ETM, SWD & JTAG) – via J-Link, Arm® Keil® ULINKTM, IAR I-jetTM, Renesas E2/E2 Lite, etc.
- User LEDs and buttons
- Three user LEDs (red, blue, green)
- Power LED (white) indicating availability of regulated power
- Debug LED (yellow) indicating the debug connection
- Two user buttons
- One reset button
- Five most popular ecosystem expansions
- MikroElektronika™ mikroBUS connector
- SparkFun® Qwiic® connector
- Two SeeedGrove® system (I2C and analog) connectors
- Two Digilent Pmod™ (SPI and UART) connectors
- Arduino™ (Uno R3) connector
- MCU boot configuration
Applications
Design & Development
Product Options
| Part Number | Status | Stock | Budgetary Price (USD) | Sampleable |
|---|---|---|---|---|
| RTK7EKA4M2S00001BE | Active | In Stock | 1u | $70.59 | Available |
Videos & Training
Kickstart IoT and embedded systems development using Renesas EK-RA4M2 and EK-RA4M3, Evaluation Kits for RA4M2 and RA4M3 MCU Groups. Familiarize yourself with the kit architecture, key features, quick start example project, and many useful resources to begin innovating quickly.
Additional Videos
News & Blog Posts
Blog Post Mar 30, 2022 |
Blog Post Jan 28, 2022 |
Blog Post Jan 28, 2022 |
Blog Post Nov 18, 2021 |
Blog Post Nov 11, 2021 |
Certifications
The EK-RA4M2 kit meets the following certifications/standards. Refer to the EK-RA4M2 user manual for the disclaimer, precautions and more details on the certifications.
EMC/EMI Standards
- FCC Notice (Class A) – Part 15
- Innovation, Science and Economic Development Canada ICES-003 Compliance: CAN ICES-3 (A)/NMB-3(A)
- CE Class A (EMC Directive 2004/108/EEC)
- Taiwan Chinese National Standard 13438, C6357 compliance, Class A limits
- Australia/New Zealand AS/NZS CISPR 32:2015, Class A
Material Selection, Waste, Recycling, and Disposal Standards
- EU RoHS
- China SJ/T 113642014, 10-year environmental protection use period
Safety Standards
- UL 94V-0
Support
Support Communities
- EK_RA4M2 Error Problem
Hello, I want to create a layer using HAL library. For example, I have a source code called App_PWM.c. This file serves as an upper layer using Timer and PWM HAL drivers. At this layer If I use local variables to execute "R_GPT_Open(&gptPWM, & ...
Apr 29, 2024 - I-003 Introduction to FSP FreeRTOS Course Materials FSP 450 EK-RA4M2
Materials for I-003 Intro to FreeRTOS Course for FSP 450 and EK-RA4M2
- Set a Pin as PWM Output for EK-RA4M2
Hello, How can I configure a pin as PWM Output Pin without using FSP Configrator?What should I add to the following codes to configure a pin for EK_RA4M2? //Set pin P405 as PWM Output. ioport_cfg_t g_ioport_cfg; ioport_pin_cfg_t g_ioport ...
Apr 19, 2024
Knowledge Base
- RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)
Last Updated: 12/14/2023 Question: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit) Answer: Renesas has equipped each EK (Evaluation Kit) for RA MCUs, such as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3 ...
Dec 14, 2023 - ICODE SLIX2 Commands
... 2 This example contains only 3 commands (Get Random Number, Set Password and Protect Page) and the project uses the SDK's RA4M2 reference implementation (EK-RA4M2 Evaluation Board). This approach involves no changes to core SDK functions or structures. The example application executes the commands in order once a ...
Oct 1, 2025 - RA and FSP Curriculum: I-003 Introduction to FSP FreeRTOS Lab
... Introduction to FSP FreeRTOS- an overview presentation covering the key features of FreeRTOS and a hands-on lab using FSP and the EK-RA6M4 or EK-RA4M2 kit. The lab illustrates the FSP implementation of key RTOS elements such as: threads/tasks, priorities, task handles, task properties, message queues ...
Aug 9, 2023