Skip to main content
Renesas Electronics Corporation

Description

The EK-RA2E2 evaluation kit enables users to effortlessly evaluate the features of the RA2E2 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2 studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life. The kit includes the EK‑RA2E2 v1 board and a micro‑USB device cable (Type‑A male to micro‑B male).

Getting Started

Running the Quick Start Example Project

  1. The EK-RA2E2 board comes pre-programmed with a quick start example project (source code provided in the EK-RA2E2 example project bundle).
  2. Power up the EK-RA2E2 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
  3. The quick start example project will begin to execute blinking the blue user LED.
  4. Refer to the EK-RA2E2 Quick Start Guide to explore additional functionality of the Quick Start example project.

Developing Embedded Applications

  1. Modifying the quick start example project – refer to the EK-RA2E2 Quick Start Guide for instructions on importing, modifying and building the quick start example project.
  2. Start with one of the many other example projects (provided in the EK-RA2E2 example project's bundle) – choose from many example projects to learn about different peripherals of the RA2E2 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.

Building Custom Hardware

  1. Start by building a functional prototype - utilize the EK-RA2E2 board with your choice of ecosystem add-ons.
  2. Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA2E2 design package.

Features

  • MCU Native Pin Access
    • R7FA2E2A72DNK MCU
    • 48MHz, Arm Cortex®-M23 core
    • 64KB Code Flash, 8KB SRAM
    • 24-pin HWQFN (4mm x 4mm x 0.8mm, 0.5mm pitch)
    • Native pin access through prototype friendly male headers
    • MCU current measurement points
  • Ecosystem & System Control Access
    • Multiple 5V input sources
      • USB (debug)
      • External power supply
    • SEGGER J-LinkTM on-board programmer and debugger
    • Debug modes
    • User LEDs and buttons
      • Three user LEDs (red, blue, green)
      • Power LED (white) indicating availability of regulated power
      • Debug LED (yellow) indicating the debug connection
      • Two user buttons
      • One reset button
    • Five most popular ecosystem expansions
      • MikroElektronika™ mikroBUS connector
      • SparkFun® Qwiic® connector
      • Two SeeedGrove® system (I2C and analog) connectors
      • Two Digilent Pmod™ (SPI and UART) connectors
      • Arduino™ (Uno R3) connector
    • MCU boot configuration

Applications

Type Title Date
Quick Start Guide PDF 1.16 MB 日本語
Manual - Development Tools PDF 1.88 MB 日本語
PCB Design Files
Log in to Download ZIP 33.61 MB
Application Note PDF 639 KB
The EK-RA2E2 example project shows how to write code for various Renesas Flexible Software Package (FSP) modules supported by the EK-RA2E2 kit. The Flexible Software Package provides an optimized, easy-to-use, scalable, and high-quality software solution for embedded system design.
Application Note PDF 2.88 MB
AI-generated Summary: The document explains how to implement a low-power data logger using RA2L1 and RA2E1 MCUs. It details the use of peripherals such as a 12-bit ADC, Data Transfer Controller, Asynchronous General-Purpose Timer, Real-Time Clock, and Event Link Controller to minimize power consumption. The system operates mainly in Software Standby and Snooze modes, performing periodic A/D conversions, level judgments, and data processing with minimal CPU activity. Data transmission occurs upon wakeup requests. The project uses Renesas e2 studio IDE and Flexible Software Package, supporting sensor inputs and analog signals. It targets applications like fitness and fleet trackers, demonstrating efficient low-power operation and data handling.
Application Note PDF 2.60 MB
AI-generated Summary: MCUboot provides a secure bootloader framework for 32-bit MCUs, enabling firmware integrity verification and secure updates. It supports multiple image upgrade methods—Overwrite, Swap, Direct execute-in-place (XIP), and RAM loading—each with distinct advantages and limitations. The RA2 MCU series uses MCUboot integrated with TinyCrypt for optimized cryptographic support, addressing limited memory constraints. The document guides creating and configuring bootloader projects, handling application updates, and running example projects on the EK-RA2E1 evaluation kit. It details development tools, hardware requirements, and best practices for secure bootloader deployment on Renesas RA2 MCUs.
Flyer PDF 412 KB
Presentation PDF 7.02 MB
Presentation PPS 24.06 MB
Flyer PDF 673 KB 日本語
Report PDF 187 KB 日本語
11 items

Software & Tools

Software & Tools

Software title
Software type
Company
RA Flexible Software Package (FSP)
FSP is an enhanced software package designed to provide easy-to-use, scalable, high-quality software for embedded system designs using Renesas RA Family of Arm Microcontrollers. Note: FSP with e² studio Installer (Platform Installer) will install the e² studio tool, FSP packs, GCC toolchain, and Segger J-Link drivers required to use this software. No additional installations are required.
Software Package Renesas
Renesas Flash Programmer (Programming GUI)
Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, RISC-V MCU, Renesas Synergy, DA1453x, DA1459x, DA1469x, DA1470x, DA148xx, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78K0R, 78K0]
Programmer (Unit/SW) Renesas
SEGGER™ J-Link™ Software and Documentation Package
Software utilities, firmware updates, and supporting documentation for the J-Link on-board programmer and debugger on the RA MCU kits.
Software Package Segger Microcontroller GmbH
QuickConnect Platform
QuickConnect platform enables fast prototyping by providing compatible hardware and software building blocks.
Software and Hardware Development Tools Renesas
4 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
[Software=RA FSP],[Board=EK-RA2E2]
Log in to Download ZIP 7.14 MB IDE: e2 studio/GCC/AC6, IAR, Keil MDK
The EK-RA2E2 example project shows how to write code for various Renesas Flexible Software Package (FSP) modules supported by the EK-RA2E2 kit. The Flexible Software Package provides an optimized, easy-to-use, scalable, and high-quality software solution for embedded system design.
Sample Code
Log in to Download ZIP 2.88 MB
Sample Code
[Toolchains=GCC Arm Embedded|10.3.1.20210824] [Software=RA FSP] [Board=EK-RA2E1]
Log in to Download ZIP 15.03 MB Compiler: GNU Arm Embedded IDE: e2 studio
3 items

Related Boards & Kits

Boards & Kits

Part NumberStatusStockBudgetary Price (USD)Sampleable
RTK7EKA2E2S00001BEActiveIn Stock1u | $49.41Available

The EK-RA2E2 kit meets the following certifications/standards. Refer to the EK-RA2E2 user manual for the disclaimer, precautions and more details on the certifications.

EMC/EMI Standards

  • FCC Notice (Class A) – Part 15
  • Innovation, Science and Economic Development Canada ICES-003 Compliance: CAN ICES-3 (A)/NMB-3(A)
  • CE Class A (EMC Directive 2004/108/EEC)
  • Taiwan Chinese National Standard 13438, C6357 compliance, Class A limits
  • Australia/New Zealand AS/NZS CISPR 32:2015, Class A

Material Selection, Waste, Recycling, and Disposal Standards

  • EU RoHS
  • China SJ/T 113642014, 10-year environmental protection use period

Safety Standards

  • UL 94V-0

Partners

Zephyr Logo
Zephyr Project

The Zephyr Project is an open-source, scalable real‑time operating system (RTOS) designed for resource-constrained embedded systems and supports a wide range of hardware architectures and development boards. For the Renesas RA4E2 Evaluation Kit, Zephyr provides focused documentation covering board features, supported peripherals, and basic build, flashing, and debugging workflows to help developers quickly get started.

See the Zephyr Project RA4E2 Evaluation Kit Documentation

Support Communities

  1. Temperature Sensor (TSN) RA2E2

    Hello,  Someone could please provide some simple example or code snippet using the internal temperature sensor (TSN) at ADC12. I am using a specific device r7fa2e2a72dnk, at the development board EK-RA2E2, at the IAR Embedded Workbench IDE. I would like a simple explanation of what to do each configuration ...

    Oct 10, 2024
  2. rs-485 DE enable is not identified as a in use pin on the Pins tab

    ... same thing happens on all mcu, not just the one Im working on at the moment. I have a project with a RA2E2 on the EK-RA2e2 board.  Im using the uart on SCI9.  In the stack setup area under properties I configured the DE pin to be enabled and ...

    Nov 14, 2025
  3. unable to read sensor through I3C but receiving proper callbacks

    ... on the FPB-RA2E2 so I was wondering if someone is able to confirm if my configurations are correct. I'm following the i3c example ek-ra2e2 projects as that project was using i3c communication between two ra2e2 boards so I'm not sure if I'm configuring the address ...

    May 31, 2023
View All Results from Support Communities (5)

Knowledge Base

  1. RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)

    Last Updated: 12/14/2023 Question: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit) Answer: Renesas has equipped each EK (Evaluation Kit) for RA MCUs, such as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3 ...

    Dec 14, 2023