Overview
The EK-RA2E1 evaluation kit enables users to effortlessly evaluate the features of the RA2E1 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life. The kit includes the EK‑RA2E1 v1 board and a micro‑USB device cable (Type‑A male to micro‑B male).
Getting Started
Running the Quick Start Example Project
- The EK-RA2E1 board comes pre-programmed with a quick start example project (source code provided in the EK-RA2E1 example project bundle).
- Power up the EK-RA2E1 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
- The quick start example project will begin to execute blinking the blue user LED.
- Refer to the EK-RA2E1 Quick Start Guide to explore additional functionality of the quick start example project.
Developing Embedded Applications
- Modifying the quick start example project – refer to the EK-RA2E1 Quick Start Guide for instructions on importing, modifying and building the quick start example project.
- Start with one of the many other example projects (provided in the EK-RA2E1 example project's bundle) – choose from many example projects to learn about different peripherals of the RA2E1 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.
Building Custom Hardware
- Start by building a functional prototype - utilize the EK-RA2E1 board with your choice of ecosystem add-ons.
- Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA2E1 design package.
Features
- MCU Native Pin Access
- R7FA2E1A92DFM MCU
- 48MHz, Arm Cortex®-M23 core
- 128KB Code Flash, 16KB SRAM
- 64-pin LQFP (10mm x 10mm x 1.7mm, 0.5mm pitch)
- Native pin access through prototype-friendly male headers
- MCU current measurement points
- Ecosystem & System Control Access
- Multiple 5V input sources
- USB (debug)
- External power supply
- SEGGER J-LinkTM on-board programmer and debugger
- Debug modes
- Debug on-board (SWD) – via J-Link
- Debug out (SWD) – via J-Link
- Debug in (ETM, SWD & JTAG) – via J-Link, Arm® Keil® ULINKTM, IAR I-jetTM, Renesas E2/E2 Lite, etc.
- User LEDs and buttons
- Three user LEDs (red, blue, green)
- Power LED (white) indicating availability of regulated power
- Debug LED (yellow) indicating the debug connection
- Two user buttons
- One reset button
- Five most popular ecosystem expansions
- MikroElektronika™ mikroBUS connector
- SparkFun® Qwiic® connector
- Two SeeedGrove® system (I2C and analog) connectors
- Two Digilent Pmod™ (SPI and UART) connectors
- Arduino™ (UNO R3) connector
- MCU boot configuration
- Multiple 5V input sources
Getting Started
Explore Ready-to-Run Solutions
Sample & Buy
Evaluation Kit for RA2E1 MCU Group
| Description: | Evaluation Kit for RA2E1 MCU Group |
| HTS (US): | 8471.50.0150 |
| ECCN (US): | 3A991.a.2 |
| SPQ: | 1 |
| Pb (Lead) Free: | No |
| Assembly Location: | UNITED KINGDOM |
Add-on Hardware
Evaluation Kit for RA2A1 MCU Group
Evaluation Kit for RA2L1 MCU Group
Evaluation Kit for RA2E2 MCU Group
Smart Lock with AWS IoT Reference Design
Videos & Training
Kickstart IoT and embedded systems development using Renesas EK-RA2E1 and EK-RA2L1, Evaluation Kits for RA2E1 and RA2L1 MCU Groups. Familiarize yourself with the kit architecture, key features, quick start example project and many useful resources to begin innovating quickly.
Additional Videos
News & Blog Posts
Blog Post Mar 25, 2022 |
Blog Post Jan 28, 2022 |
Blog Post Jan 28, 2022 |
Blog Post Nov 18, 2021 |
Blog Post Nov 11, 2021 |
Support
Support Communities
- I2C Master transmission fails if I2C Slave Driver is added to the project stack (EK-RA2E1)
HI ! This can be easily verified with the I2C Master example. Example works, data is fine (valid I2C packet). After adding the slave driver (just adding in stacks without modification and generate), the same R_IIC_MASTER_Write fails: no valid start condition anymore! The slave driver is not opened ...
Jul 15, 2021 - Sleep current is not stable with RTC in Dev kit EK-RA2E1
Hi , I would like to verify the sleep performance of RA2E1 series MCU. Hence I have a program which puts MCU into software standby mode and wakes up using RTC alarm MCU goes to software standby mode and current consumption is at 0.65uA and starts increase and not stable ...
Jan 14, 2022 - RTC not working in Dev kit EK-RA2E1
Hi , I have modified example code to periodically interrupt for every 1 second. However I am not getting RTC interrupt . Following is the code snippet. /*******************************************************************************************************************//** * The RA Configuration tool generates main() and uses it to generate threads if an RTOS is used. This function is * called by ...
Jan 12, 2022
Knowledge Base
- RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)
Last Updated: 12/14/2023 Question: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit) Answer: Renesas has equipped each EK (Evaluation Kit) for RA MCUs, such as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3 ...
Dec 14, 2023