Skip to main content
Renesas Electronics Corporation

Renesas Blog

Provisioning App Blog image

Renesas Wi-Fi Provisioning App is Available Now on Google and Apple Stores

Renesas’ Wi-Fi Provisioning App, a mobile application that works with development kits supported by the DA16200 and DA16600 Wi-Fi SoCs, is now available for use on Google Play and Apple Stores.

FreeRTOS Support for Its Ultra-low Power DA16200 SoC Blog Image

Renesas Introduces FreeRTOS Support for Its Ultra-low Power DA16200 SoC

Renesas offers FreeRTOS support for the DA16200, a real-time operating system for MCUs that helps to program, use, secure, connect, and manage small, low-power edge devices without extra effort.

Multi-Cell USB-PD + QC2 & QC3 Power Bank Blog

Multi-Cell USB-PD and PPS Power Bank with Qualcomm Quick Charge and OS Independent Monitoring

/node/1601921This is a detailed description of a solution for a multi-cell USB Power Delivery (USB-PD) enabled power bank using a 2S to 4S battery stack that supports USB-PD 3.0, PPS and Qualcomm Quick Charge.

Develop Faster Using Example Projects for RA MCU Innovation Kits for IoT

Develop Faster Using Example Projects for RA MCU Innovation Kits for IoT

Users of RA MCU innovation kits for IoT can utilize 600+ example projects as building blocks to create feature-rich IoT and embedded proof-of-concepts quickly and easily.

Quickly Programming RA MCU Innovation Kits for IoT

Quickly Programming RA MCU Innovation Kits for IoT

This blog provides useful information on programming a pre-built hex file onto an RA kit using Renesas Flash Programmer and Segger® J-Flash Lite without having to build the source code or use an IDE.

hybrid, power line communication plus sub-GHz RF reference platform (Y-G-HYBRID-PLC-RF)

Renesas Launches its First Hybrid Reference Platform Combining Power Line Communication and Sub-GHz Radio

Renesas’ first hybrid, power line plus sub-GHz RF reference platform is a reference board that supports all key communication protocols such as WiSUN, G3-PLC, G3-PLC Hybrid, PRIME 1.3.6 + 1.4, PRIME Hybrid and Meters and More.

What is Driving DDR5? Blog

What is Driving DDR5?

This blog goes over the need for faster and more memory and how DDR5 is addressing this need.

The RA MCU family is made to help solve your design challenges

The RA MCU Family is Made to Help Solve Your Design Challenges

The entry-level RA4E1 and RA6E1 MCUs address key design challenges including the optimal balance between performance and power consumption, as well as seamless migration options for future designs.

RA Book Features Blog

Get Where You’re Going with the Official Renesas RA Family Guide

This blog presents the RA Family Beginner’s Guide – A step-by-step guide that takes you from the basics of the FSP and RA toolchain to creating a project from scratch with the EK-RA6M4 evaluation kit.

Robotic Lawn Mower Blog

Lawn Maintenance Getting You Down? Robotic Mowers to the Rescue!

Compared to conventional lawn mowers, robotic lawn mowers offer many benefits including they are better for our environment and offer the convenience of remote programming, controlling and monitoring.