Skip to main content
Renesas Electronics Corporation

AI Goes Horizontal—Analog Goes Deep

Image
Blog author photo of Karthi Gopalan.
Karthi Gopalan
VP of Business Strategy
Published: May 8, 2026

An AI-driven gadget that acts on a drifting signal doesn't know it's wrong. It just acts—confidently, precisely, and in the wrong direction. Confidence without accuracy isn't intelligence. It's a liability.

The gap between what a system is told and what is actually happening in the physical world is closed by one thing: the analog foundation beneath it, and that foundation is everywhere.

Artificial intelligence has become the operating layer of the entire physical world, embedded in factories, vehicles, robots, satellites, and data centers. AI has gone horizontal, but beneath every intelligent system, there is a foundation that makes it all possible. That foundation is analog.

While the industry debates models, parameters, and computer architectures, a quieter and more consequential story is unfolding at the signal level. Every autonomous system, no matter how sophisticated its software, must ultimately sense the real world, respond to it, and act within it. The interface between the physical and the digital is analog, and as systems grow more intelligent, that interface doesn't just grow, it multiplies.

By "signal chain," I mean the end-to-end path from sensors through analog front ends, conversion, synchronization, power, and control up to the data the model actually sees.

The question is no longer whether AI runs at the edge. The question is whether the analog foundation beneath it is deep enough, not just to make it trustworthy, but to make it fast, precise, and capable of performing at the highest level the application demands.

The Analog Attach Curve

To see what that means in practice, it helps to name the pattern that shows up every time physical AI moves from prototypes to production.

There is a pattern that repeats across every domain where physical AI is taking hold. As machines grow more capable, autonomous, precise, and safety-critical, the analog and mixed-signal content required to run them does not grow linearly, it compounds.

Image
Table showing Analog IC content needed per platform and at specified depth.

Note: Multipliers are directional and illustrative, to show the shape of the curve.

Image
Graph showing how analog IC content is proportional to autonomy.

Figure 1. Analog IC Content ∝ Autonomy

In Figure 1, as autonomy rises, analog content compounds: more sensor interfaces, more data converters, more motor-control channels, more power rails, and tighter safety monitoring.

The humanoid is where the curve makes its fullest argument. Every gesture, every step, every decision traces back through more than 200 analog ICs spanning motor control at every joint, position sensing, torque and force feedback, power management, and a perception layer covering LiDAR, vision, touch, pressure, and impedance. At the fingertip, where millimeters and milliseconds determine whether a grasp succeeds, the architecture replicates itself again. Intelligence rises. The signal chain deepens with it, and at every layer, the demand is not merely for a signal that is good enough to trust, it is for a signal that is accurate enough, fast enough, and stable enough to perform.

Image
Illustration showing the quantity of ICs spanning motor control at every joint of a humanoid.

Figure 2. Quantity of ICs Spanning Motor Control at Every Joint of a Humanoid

Image
Graphic showing the signal chain anatomy for a humanoid-platform.

Figure 3. Humanoid Platform Signal Chain Anatomy

A humanoid's signal chain repeats at every joint: motor drive and current sensing, position feedback (encoders/resolvers), torque/force feedback, local power management, and high-integrity communications—extending to fingertip pressure/impedance sensing for stable grasp. Analog is not beneath AI. It is what makes AI physical. And Renesas is built, end-to-end, to deliver it.

Why Horizontal Scale Without Vertical Depth Breaks

Industrial environments are electrically hostile. Temperature swings, vibration, electromagnetic noise, and long cable runs degrade signal quality in ways software cannot compensate for after the fact. A position sensor that drifts by half a degree under thermal stress doesn't generate an error flag, it generates a wrong answer that the AI system acts on with full confidence.

This is the gap between AI that performs in the lab and AI that performs in the field.

Bridging requires not just components but an end-to-end signal architecture where sensing, control, power, and connectivity are engineered to work as one system, not bolted together as an afterthought.

In physical AI, accuracy isn't a single spec—it's a system property. It lives in calibration, timing, power integrity, and fault-aware control.

The Decade Ahead

The systems that win won't be the ones with the largest models. They will be the ones that deliver the most reliable performance in the real world across temperature, vibration, latency, noise, power budgets, safety constraints, and long lifecycles.

That is not a software problem. It is a signal chain problem. If you're building physical AI, treat analog as a first-class design axis: architect it early, budget for it explicitly, and engineer sensing, control, power, and connectivity as one system, not a pile of parts.

Key Takeaways

  • As autonomy increases, analog and mixed-signal depth compounds—performance, precision, and reliability become determinant, not just model size.
  • The field breaks systems through drift, EMI, vibration, and cable losses—upstream signal integrity errors look like "confident" AI mistakes.
  • Winning architecture treats sensing, control, power, and connectivity as one engineered signal system—designed early, budgeted explicitly, and built for the real world.

AI goes horizontal. The winners go deep. That race is already underway.

Resources

Visit renesas.com/analog to dive deeper.