- First-of-its kind bidirectional GaN technology with DC blocking dramatically reduces switch count needed for power conversion topologies
- Compatible with standard gate drivers
- Soft- and hard-switching capable, with fast, clean transitions
TOKYO, Japan and SAN ANTONIO ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the industry’s first bidirectional switch using depletion-mode (d-mode) GaN technology, capable of blocking both positive and negative currents in a single device with integrated DC blocking. Targeting single-stage solar microinverters, AI data centers and onboard electric vehicle chargers, the high-voltage TP65B110HRU dramatically simplifies power converter designs and replaces conventional back-to-back FET switches with a single low-loss, fast-switching, easy-to-drive device.
Single-Stage Topology Boosts Efficiency, Reduces Components
Today’s high-power conversion designs use unidirectional silicon or silicon carbide (SiC) switches, which block current in only one direction when in the off state. As a result, power conversion must be divided into stages with multiple switched bridge circuits. For example, a typical solar microinverter uses a four-switch full bridge to convert from DC to DC for the first stage, followed by a second stage to produce the final AC output to the grid. Even as the electronics industry moves toward more efficient single-stage converters, engineers must work around inherent switching limitations. Many of today’s single-stage designs use conventional unidirectional switches back-to-back, resulting in a four-fold increase in switch count and reduced efficiency.
Bidirectional GaN changes this landscape entirely. By integrating bidirectional blocking functionality on a single GaN product, power conversion can be achieved in a single stage using fewer switching devices. A typical solar microinverter, for example, will require only two high-voltage Renesas SuperGaN® bidirectional devices, eliminating the intermediary DC-link capacitors and cutting the switch count by half. In addition, GaN products switch fast, with low stored charge, enabling higher switching frequencies and higher power density. In a real-world single-stage solar microinverter implementation, the new GaN architecture demonstrated higher than 97.5% power efficiency with the elimination of back-to-back connections and slow silicon switches.
Combining Robust Performance and Reliability with Silicon-Compatible Drivers
Renesas field-proven 650V SuperGaN devices are based on a proprietary normally-off technology that is simple to drive and highly robust. The TP65B110HRU combines a high-voltage bidirectional d-mode GaN chip co-packaged with two low-voltage silicon MOSFETs with high threshold voltage (3V) high gate margin (±20V) and built-in body diodes for efficient reverse conduction. Compared with enhancement mode (e-mode) bidirectional GaN devices, the Renesas bidirectional GaN switch offers compatibility with standard gate drivers that require no negative gate bias. This translates to a simpler, lower-cost gate loop design and fast, stable switching in both soft and hard switching operation without a performance penalty. Power conversion topologies that require hard switching, such as the Vienna-style rectifier, can benefit from its high dv/dt capability of >100 V/ns, with minimum ringing and short delays during on/off transitions. The Renesas GaN device enables true bidirectional switching with high robustness, high performance and ease of use.
“Extending our SuperGaN technology to the bidirectional GaN platform marks a major shift in power conversion design norms,” said Rohan Samsi, Vice President, GaN Business Division at Renesas. “Customers can now achieve higher efficiency with fewer switching components, smaller PCB area and lower system cost. At the same time, they can accelerate design by leveraging Renesas’ system-level integration with gate drivers, controllers and power management ICs.”
Key features of the TP65B110HRU:
- ±650V continuous peak AC and DC rating, ±800V transient rating
- 2kV Human Body Model ESD protection rating (HBM and CDM)
- 110 mΩ typical RSS,ON @ 25⁰C
- 3V typical Vgs(th)
- No negative drive required
- ±20V maximum Vgs
- >100 V/ns dv/dt immunity
- 1.8V, VSS,FW freewheeling diode voltage-drop
- TOLT top-side cooled package with industry standard pin-out
Renesas will showcase the latest bi-directional GaN switch and its growing portfolio of intelligent power solutions in booth #1219 at the Applied Power Electronics Conference (APEC), in San Antonio, Texas, March 22-26, 2026.
Availability
The TP65B110HRU bi-directional GaN switch is available in quantity today. Customers can also purchase the RTDACHB0000RS-MS-1 evaluation kit for testing with different drive options, detect AC zero crossings and implement ZVS soft switching.
Winning Combinations
Renesas offers 500W Solar Microinverter and Three-Phase Vienna Rectifier System solutions that combine the new GaN bi-directional switch with numerous compatible devices from its portfolio. These Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. More than 400 Winning Combinations with a wide range of products from the Renesas portfolio enable customers to speed up the design process and bring their products to market more quickly. They can be found at renesas.com/win.
Get Powered by Renesas
Driven by innovation, quality and reliability, Renesas leads the way in power electronics, shipping more than four billion parts per year from our portfolio of power management ICs, discrete and wide-bandgap GaN products, computing power devices and many more. These products span all major segments including automotive, IoT, infrastructure and industrial applications. Our power portfolio seamlessly attaches to our leading MCU, MPU, SoC and analog solutions, simplifying and accelerating the design process with hundreds of engineering-vetted Winning Combinations and innovative tools such as PowerCompass™ and PowerNavigator™ design software. Find out more at renesas.com/power.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.
(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.