Skip to main content
Renesas Electronics Corporation

Renesas Launches 64-bit RZ/G3L and RZ/G3SE MPUs for Advanced HMI and IoT Edge Systems

September 10, 2026
  • Pin-compatible MPUs enable scalable design on common PCB
  • 1 mW-level standby power and fast Linux wakeup enable always-connected applications
  • PCIe and TSN-capable Ethernet provide high-speed connectivity and flexible system expansion

TOKYO, Japan, September 10, 2026 ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its RZ/G Series with new 64-bit general-purpose microprocessors (MPUs) for Human Machine Interface (HMI) and IoT edge systems. The RZ/G3L and RZ/G3SE are pin-compatible MPUs that support a broad range of industrial and consumer HMI and IoT gateway and home gateway systems requiring high processing performance and high-speed network connectivity.

The RZ/G3L integrates a GPU (Graphics Processing Unit) for 3D graphics rendering along with an H.264 video codec. This combination is ideal for powering smart retail terminals and medical HMI devices that demand rich graphics and video capabilities. The RZ/G3SE is designed for IoT devices with basic display requirements, such as EV chargers and industrial gateway devices that provide status indicators and configuration screens. Because the RZ/G3L and RZ/G3SE are pin-compatible, developers can reuse a PCB design across multiple product variants, simplifying development and reducing time to market.

High Performance with 1 mW-Level Standby Power

These new products deliver high processing performance with a CPU cluster incorporating up to four Arm® Cortex®-A55 cores running at up to 1.2 GHz, together with a Cortex-M33 coprocessor running at 200 MHz. At the same time, the third-generation RZ/G Series adopts a proprietary power management architecture that significantly reduces standby power. As a result, the new products can lower standby power to the 1 mW level in deep standby mode. They can remain in standby mode while retaining the Linux system in memory and resume operation quickly when needed. These power-saving features are well-suited for industrial and IoT devices that require always-on connectivity.

High-Speed Connectivity for Expanded System Capabilities

Equipped with high-speed interfaces such as PCIe, TSN-capable Gigabit Ethernet and USB, the new MPUs allow developers to add application-specific features and connectivity options. PCIe supports connectivity to 5G communication modules, Wi-Fi 6 modules and even external AI accelerators. TSN-capable Gigabit Ethernet enables low-latency and highly reliable communications required in industrial networks, where real-time performance is critical.

"As industrial and IoT devices grow more sophisticated, customers need to balance performance, power consumption, connectivity and design scalability,” said Hari Pendurty, Vice President of the EP Edge AI and Application Processors Business Division at Renesas. “The RZ/G3L and RZ/G3SE were developed to help customers meet these evolving requirements and scale products more efficiently by leveraging a common hardware platform across different applications.”

A Rich Ecosystem Accelerates Development

Renesas offers ten ecosystem solutions, including GUI development environments, operating systems (OS), software and system-on-modules (SoMs). Renesas will continue to expand the ecosystem toprovide customers with a broader range of validated software, tools and hardware solutions.

For other partners, please see the Renesas Partner Program.

Additional Features

  • Main CPU in quad-core or dual-core configurations
  • Available in 14 mm square 400-pin LFBGA and 17 mm square 368-pin LFBGA packages
  • ECC (error checking and correction) on both on-chip memory and the external DDR interface
  • Comprehensive security features, including Renesas Secure IP, Secure Boot, Arm TrustZone, and tamper detection
  • Wide operating temperature range from –40°C to +125°C
  • Verified Linux Package (VLP) compliant with the trusted Civil Infrastructure Platform (CIP) for long-term support

Winning Combinations

Renesas has combined the new MPUs with numerous compatible devices from its portfolio to offer a wide range of solutions. These include the Mode3 AC EV Charger Wallbox with High-Level PLC Communication based on the RZ/G3L, as well as the AI-Enabled Smart Home Security Hub based on the RZ/G3SE, which enables advanced monitoring through integration with cameras, microphones, and sensors, along with cloud connectivity. For other Winning Combinations, please visit renesas.com/win.

Availability

The RZ/G3L and RZ/G3SE are available today. An evaluation board kit, consisting of a SMARC v2.1 module board and a carrier board, is also available for both devices. More information is available at https://www.renesas.com/rzg3l and https://www.renesas.com/rzg3se.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.