Skip to main content
Renesas Electronics Corporation

Renesas Introduces Industry’s Highest Performance Entry-Line MCUs

New RA6E1 Group Based on Arm® Cortex®-M33 Delivers 200 MHz Performance in Addition to Low Power Performance , basic_html

September 30, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced a new Group of 32-bit microcontrollers (MCUs) in its RA Family. The new RA6E1 MCUs, based on the Arm® Cortex®-M33 core, are the industry’s first Entry-Line MCUs to deliver 200 MHz performance. The new devices also provide exceptional low power consumption specifications, along with a rich list of peripheral features.

Renesas’ RA Family MCUs are differentiated by a unique combination of very low power consumption, best-in-class security options, including Arm TrustZone® technology, and Renesas’ Flexible Software Program (FSP) that supports all RA Family offerings. The FSP includes highly efficient drivers and middleware to ease the implementation of communications and security. The FSP’s GUI simplifies and accelerates the development process. It enables flexible use of legacy code, as well as easy compatibility and scalability with other RA Family devices. Designers using FSP also have access to the extensive Arm ecosystem, offering a wide range of tools that help speed time-to-market, as well as Renesas’ extensive partner network.

“Our RA Family is setting new standards in the market for Entry-Line MCUs with unprecedented performance,” said Roger Wendelken, Senior Vice President in the IoT and Infrastructure Business Unit at Renesas. “With the new RA6E1 Group we developed an MCU which is an exceptional fit for calculation-intensive IoT applications requiring both high performance and the lowest power, as well as the need for value-optimized feature integration and connectivity.”

The RA6E1 Group MCUs includes six different parts, spanning from 48-pin to 100-pin packages, and from 512kB to 1MB of flash memory along with 256kB of SRAM. The RA6E1 devices offer exceptional power consumption specifications, and extensive peripherals and connectivity options (including Ethernet), delivering a unique combination of performance and features.

Key Features of the RA6E1 Group

  • 200 MHz Arm Cortex-M33 CPU core
  • Integrated flash memory options from 512KB to 1MB; and 256KB RAM
  • Support for wide temperature range: Ta = -40/85°C
  • Package options from 48- to 100-pin
  • High performance: 3.95CoreMark / MHz executing the CoreMark Algorithm from embedded Flash
  • Integrated Ethernet (with integrated MAC)
  • Integrated USB 2.0 Full-Speed, serial communication (SCI with flexible synchronous and asynchronous modes, I2C, SPI), CAN, SSI, SDHI, QSPI
  • Integrated Renesas Timer
  • Advanced Analog

Renesas has combined the RA6E1 MCUs with complementary analog and power offerings that work together seamlessly to create Winning Combinations for a variety of applications. Examples of these Winning Combinations include a Ultra-small Finger Print Sensor and a Cloud Gateway Module. Renesas offers more than 250 Winning Combinations with compatible devices for a wide range of applications and end products. They can be found at renesas.com/win.

Availability

All the new RA6E1 MCUs are available today. To help engineers get started with the RA6E1 MCUs, Renesas is offering the FPB-RA6E1 Fast Prototype Board with an on-chip debugger, priced in the 20 USD range. More information is available at renesas.com/RA6E1. More details about the new Fast Prototyping Board can be found at: renesas.com/FPB-RA6E1.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.

(Remarks). Arm, Arm Cortex and TrustZone are trademarks or registered trademarks of Arm Limited in the EU and other countries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.