Skip to main content
Renesas Electronics Corporation

Renesas Expands RL78 Family with Ultra-Low-Power 16-Bit RL78/G21 MCU Optimized for Smart Appliance System Control

October 28, 2026
  • Extends proven low-power leadership by cutting down power consumption by half, achieving top ULPMark®-PeripheralProfile benchmark scores, and increasing reliability with ±4 kV HBM ESD tolerance.
  • Expands the existing RL78/G23 lineup with expanded touch-key functionality for advanced HMI devices, along with enhanced security.

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the RL78/G21, a new member of its RL78 family. Renesas holds the No. 1 global market share in 16-bit MCUs (Note 1). The RL78/G21 MCU extends that leadership into the next generation of smart appliances. Optimized for smart system control, the new MCU product series RL78/G21 combines a low-power design with optimized peripheral functions enabling both energy savings and lower costs in system-control applications such as air conditioners, refrigerators, washing machines and microwave ovens.

Renesas also expanded its existing RL78/G23 lineup with new devices featuring additional capacitive-touch channels to address demand for more advanced HMI devices. Together, the RL78/G21 and RL78/G23 provide flexible design options: RL78/G21 optimized for efficient system-control, while RL78/G23 integrates system control and user-interface functions into a single MCU, helping reduce system BOM costs.

Ensuring Reliability, Security and Flexibility in Smart Appliances

For more than 15 years, the RL78 family has earned the trust of customers worldwide across a broad range of applications. The new RL78/G21 and RL78/G23 strengthen that foundation forward with enhanced security capabilities that help protect against physical threats, such as counterfeiting and cloning, as well as cyber threats, including unauthorized access, information leakage, tampering and spoofing. The RL78/G21’s high electrostatic discharge (ESD) tolerance of ±4 kV HBM contributes to higher reliability throughout manufacturing and assembly, as well as during operation of the end product. The RL78/G21 also adds the UARTA communication interface, an upgrade over the RL78/G13, enabling flexible system expansion such as the addition of sensors. Because the RL78/G21 is pin and function compatible with the existing RL78/G13 and RL78/G23, customers can transition designs seamlessly to the new devices with minimal redesign effort.

Ultra-Low-Power MCU Optimized for System Control

The RL78 family has demonstrated its ultra-low-power capabilities with products achieving top scores in the ULPMark®-PeripheralProfile benchmark. Leveraging the advanced low-power technologies developed for the RL78 family, the RL78/G21 achieves an operating current of just 34 μA/MHz, nearly half that of the leading RL78/G13 MCU products. This helps reduce battery capacity, downsize power supply circuits and lower overall system costs. Optimization for system control also gives the device strong price competitiveness in the class of products with 128KB or 256KB of code flash memory. The integration of a high-speed on-chip oscillator (HOCO) with ±1.0% accuracy and 4KB of data flash eliminates the need for an external oscillator and EEPROM, reducing BOM costs.

Scalable Touch HMI Support

As demand for touch input grows with the increasing sophistication of human-machine interfaces (HMIs), Renesas expanded the RL78/G23 lineup with the RL78/G23 (R7F104G), which offers enhanced capacitive-touch sensing. Compared with the existing RL78/G23 (R7F100G), which provides 14 touch channels in the 44-pin version and 16 touch channels in the 48-pin version, the new devices significantly increase the number of touch channels to 24 and 25, respectively. Renesas provides common touch peripheral functionality and the QE for Capacitive Touch tool across the RL78, RX and RA families, enabling scalable HMI development ranging from simple user interfaces to advanced graphics displays.

"The RL78/G21 and RL78/G23 are built on the proven strengths of the RL78 family, delivering significant advances in low-power performance, reliability and security,” said Raji Mukhopadhyay, Business Division Manager, EP Mainstream MCU Business Division at Renesas. “The RL78/G21’s ±4 kV HBM ESD tolerance is a key differentiator. It further strengthens reliability, while its enhanced security capabilities address the growing need for more secure smart appliances.”

Additional Features

  • Self-diagnostic functionality enabled by an IEC 60730-compliant self-test library
  • Security features including flash read protection, flash shield window, Unique ID and Customer ID
  • High ESD tolerance of ±4 kV HBM (Human Body Model) (RL78/G21 only)
  • Pin and functional compatibility with the existing RL78/G13 and RL78/G23
  • Wide operating voltage range from 1.6V to 5.5V
  • Development support through Smart Configurator and the Fast Prototyping Board (FPB)

“Appliance makers are asking for more intelligence, better user experiences and stronger security without increasing cost or energy consumption,” added Mukhopadhyay. “With the RL78/G21’s ultra-low-power performance and enhanced security, alongside the RL78/G23’s expanded touch capabilities, customers can select the right MCU for their system-control and HMI requirements and bring more efficient, reliable and secure smart appliances to market faster.”

Winning Combinations

Renesas combines the RL78/G21 and RL78/G23 with various devices from its portfolio to offer smart appliance solutions, including Smart Remote-Controlled Tankless Gas Water Heater and Household Water Pump. For other Winning Combinations, please visit renesas.com/win.

Availability

The new RL78/G21 and RL78/G23 products are available today. Pricing for the RL78/G21 starts at US$0.56 for the 128KB/44-pin LQFP product and US$0.77 for the 256KB/44-pin LQFP product (Note 2). More information is available at https://www.renesas.com/rl78g21 and https://www.renesas.com/rl78g23.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

Note 1: Source: Gartner®, Market Share: Semiconductors by End Market, Worldwide, 2025. Rajeev Rajput et al., 17 March 2026. 16-bit MCUs = Microcontroller 16-bit in 2025
Gartner does not endorse any company, vendor, product or service depicted in its publications, and does not advise technology users to select only those vendors with the highest ratings or other designation. Gartner publications consist of the opinions of Gartner’s business and technology insights organization and should not be construed as statements of fact. Gartner disclaims all warranties, expressed or implied, with respect to this publication, including any warranties of merchantability or fitness for a particular purpose.
GARTNER is a trademark of Gartner, Inc. and its affiliates.

Note 2: Suggested resale pricing is provided for reference only and is based on a 10,000-unit purchase quantity in U.S. dollars. Please contact your nearest Renesas sales representative or distributor for an actual quotation.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.