Skip to main content
Renesas Electronics Corporation

Renesas Adds Two New MCU Groups to Blazing Fast RA8 Series with 1GHz Performance and Embedded MRAM

RA8M2 Devices Address General-Purpose Applications and RA8D2 Devices Target High-End Graphics and HMI; Both Offer Dual-Core Options for Even More Horsepower, basic_html

October 22, 2025

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the RA8M2 and RA8D2 microcontroller (MCU) groups. Based on a 1 GHz Arm® Cortex®-M85 processor with an optional 250 MHz Arm® Cortex®-M33 processor, the new MCUs are the latest Renesas offerings to deliver an unmatched 7300 Coremarks of raw compute performance, the industry benchmark for MCUs. The optional Cortex-M33 processor enables efficient system partitioning and task segregation.

Both RA8D2 and RA8M2 devices are ultra-high performance MCUs as part of the second generation of the RA8 Series – the RA8M2 are general-purpose devices, and the RA8D2 MCUs are packed with a variety of high-end graphics peripherals. They are built on the same high-speed, low-power 22-nm ULL process used for the RA8P1 and RA8T2 devices introduced earlier this year. The devices include single and dual core options, and a specialized feature set to address the needs of a broad base of compute intensive applications. They take advantage of the high performance of the Arm Cortex-M85 processor and Arm’s Helium™ technology to offer a significant performance boost for digital signal processor (DSP) and machine learning (ML) implementations.

The RA8M2 and RA8D2 devices offer embedded MRAM that has several advantages over Flash technology - high endurance & data retention, faster writes, no erase needed, and byte addressable with lower leakage and manufacturing costs. SIP options with 4 or 8 MB of external flash in a single package are also available for more demanding applications. Both the RA8M2 and RA8D2 MCUs include Gigabit Ethernet interfaces and a 2-port TSN switch to address industrial networking use cases.

Both of the MCU Groups provide a combination of the high performance of the Cortex-M85 core, together with large memory and a rich peripheral set, making them particularly suitable for a wide range of IoT and industrial use cases. The lower power CM33 core can act as a housekeeping MCU, executing system tasks while the high performance CM85 core stays in sleep mode, to be woken up only as needed for high compute tasks, thus lowering the system power consumption.

“The RA8M2 and RA8D2 complete Renesas’ new generation of RA8 MCUs, purpose-built for the high-performance microcontroller market,” said Daryl Khoo, Vice President of the Embedded Processing Marketing Division at Renesas. “This portfolio empowers Renesas to deliver scalable, secure and AI-enabled embedded processing solutions that accelerate customer innovation and time-to-market across a broad spectrum of industrial, IoT and select automotive applications. Renesas’ commitment to innovation is reflected in the RA8 Series’ ability to address complex processing requirements while maintaining lower power consumption and minimizing total cost of ownership to future-proof customers’ designs.”

RA8D2 Feature Set Optimized for Graphics and HMI Applications

The RA8D2 MCUs provide a plethora of features and functions for graphics and HMI applications:

  • High resolution Graphics LCD Controller supports up to 1280x800 displays with both parallel RGB and 2-lane MIPI DSI interfaces
  • Two-Dimensional Drawing Engine offloads the graphics rendering tasks from the CPU and supports graphics primitives
  • Multiple camera interface options enable camera and vision AI applications,
    • 16-bit camera interface (CEU) with support for image data fetch, processing and format conversion
    • MIPI CSI-2 interface offers a low pin-count interface with 2 lanes, each up to 720Mbps
    • A VIN module performs vertical and horizontal scaling and format and color space conversions of YUV and RGB data inputs received from the MIPI CSI-2 interface
  • Audio interfaces such as I2S and PDM support digital microphone inputs for audio and voice AI applications
  • Comprehensive graphics solution with industry-leading embedded graphics GUI packages from SEGGER emWin and Microsoft GUIX, integrated into Renesas’ FSP
  • Software JPEG decoder optimized for Helium, available with both emWin and GUIX solutions, allows decode of JPEG images with up to 27fps end-to-end graphics performance with Helium acceleration
  • Multiple graphics ecosystem partners such as Embedded Wizard, Envox, LVGL and SquareLine Studio are offering solutions that employ RA8D2 using Helium to accelerate graphics functions and JPEG decoding

Key Features of the RA8M2 and RA8D2 Group MCUs

  • Core: 1 GHz Arm Cortex-M85 with Helium; Optional 250 MHz Arm Cortex-M33
  • Memory: Integrated 1MB high-speed MRAM and 2MB SRAM (including 256KB TCM for the Cortex-M85 and 128KB TCM for the M33). 4MB and 8MB SIP devices coming soon.
  • Analog Peripherals: Two 16-bit ADC with 23 analog channels, two 3-channel S/H, 2-channel 12-bit DAC, 4-channel high-speed comparators
  • Communications Peripherals: Dual Gigabit Ethernet MAC with DMA, USB2.0 FS Host/Device/OTG, CAN2.0 (1Mbps)/CAN FD (8Mbps), I3C (12.5Mbps), I2C (1Mbps), SPI, SCI, Octal serial peripheral I/F
  • Advanced Security: RSIP-E50D Cryptographic engine, robust secure boot with FSBL in immutable storage on-chip, secure debug, secure factory programming, DLM support, tamper protection, DPA/SPA protection,

The new RA8M2 and RA8D2 Group MCUs are supported by Renesas’ Flexible Software Package (FSP). The FSP enables faster application development by providing all the infrastructure software needed, including multiple RTOS, BSP, peripheral drivers, middleware, connectivity, networking, and security stacks as well as reference software to build complex AI, motor control and cloud solutions. It allows customers to integrate their own legacy code and choice of RTOS (FreeRTOS and Azure RTOS) with FSP, thus providing full flexibility in application development. In addition, Zephyr support is now included. Using the FSP will ease migration of existing designs to the new RA8 Series devices.

Winning Combinations

Renesas has combined the new RA8 Group MCUs with numerous compatible devices from its portfolio to offer a wide array of Winning Combinations, including the Smart Glasses and Pet Camera Robot for the RA8M2, and both Ki Wireless Power Transceiver System (Tx) and Ki Wireless Power Receiver System (Rx) for the RA8D2. Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly. They can be found at renesas.com/win.

Availability

The RA8M2 and RA8D2 Group MCUs are available now, along with the FSP software. The RA8M2 devices are available in 176-pin LQFP, 224-pin and 289-pin BGA packages. The RTK7EKA8M2S00001BE Evaluation Kit is also available. The RA8D2 MCUs are offered in 224-pin and 289-pin BGA packages. The RTK7EKA8D2S01001BE Evaluation Kit supports the RA8D2 devices. Information on all these offerings is available at www.renesas.com/RA8M2 and www.renesas.com/RA8D2.

Renesas MCU Leadership

The world leader in MCUs, Renesas ships more than 3.5 billion units per year, with approximately 50% of shipments serving the automotive industry, and the remainder supporting industrial and Internet of Things applications as well as data center and communications infrastructure. Renesas has the broadest portfolio of 8-, 16- and 32-bit devices, delivering unmatched quality and efficiency with exceptional performance. As a trusted supplier, Renesas has decades of experience designing smart, secure MCUs, backed by a dual-source production model, the industry’s most advanced MCU process technology and a vast network of more than 250 ecosystem partners. For more information about Renesas MCUs, visit renesas.com/MCUs.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.