Image
Keita Kashima
Keita Kashima
IoT Product Marketing

Do you know that RX family supports Microsoft Azure RTOS? Azure RTOS has a certification program which ensures the operation of Azure RTOS works on certified evaluation kits. Our development kits, RX65N-Cloud-Kit and RX65N-2MB-Starter-Kit-Plus, have obtained this certification.

Image
Azure-Certified-Device
Image
rx65n-cloud-kit

RX65N Cloud Kit | Azure Certified Device catalog(https://devicecatalog.azure.com/)

Image
rsk-for-rx65n-2mb

Renesas Starter Kit+ for RX65N-2MB | Azure Certified Device catalog(https://devicecatalog.azure.com/)

In recent years, major cloud venders are providing cloud solutions including Real-time operating system (RTOS), making it easier for edge devices to connect to the cloud.

In addition to FreeRTOS for AWS cloud service, RX family now also supports Azure RTOS and offers an environment where you can easily connect to Microsoft Azure.

If you are considering using Azure, please try the sample code of RX family MCU provided in Azure RTOS Git Hub in the link below.

https://github.com/azure-rtos/samples

Image
Azure RTOS - Additional samples

In our development environment e2 studio, you can download the latest version of Azure RTOS and create/build a project quickly by following the instructions on the project creation screen.
 

Image
Instructions on the project creation-screen

Using sample code provided, it enables connection to the Azure IoT Hub and data can be transferred to the cloud.

It is also possible to display the data on the dashboard.
 

Image
Dashboard

We have many more solutions which are not introduced in this article. Please vist below link to get more information about RX family cloud solution and samples code.

https://www.renesas.com/rx-cloud

We are planning to obtain Azure Certification for other evaluation boards such as RX72N. There is also a plan for hands-on seminar for Azure IoT. Please stay tune to find out our next information.

Share this news on

Log in or register to post comments

Share this news on