Skip to main content
Renesas Electronics Corporation

Renesas Electronics Launches RX72M Group of Microcontrollers with EtherCAT® Support for Industrial Applications

Delivers RX Family’s Highest Performance and Memory Capacities While Realizing Control and Communication Functions on a Single Chip , basic_html

June 6, 2019

TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced the RX72M Group of RX microcontrollers (MCUs) featuring an EtherCAT® slave controller for industrial Ethernet communication. The new flagship product group for the Renesas RX family offers a high-performance, single-chip MCU solution with large memory capacities for industrial equipment requiring control and communication functions such as compact industrial robots, programmable logic controllers, remote I/O, and industrial gateways.

The use of EtherCAT in industrial Ethernet is growing fast, and is currently used on dedicated MCUs, ICs, and high-end system-on-chip (SoC) devices specialized for EtherCAT communication. The new RX72M Group achieves the superior performance of a 1396 CoreMark® score (Note 1) at 240MHz as measured by EEMBC® Benchmarks, and it is capable of both application processing and EtherCAT communication. Combining a motor-control MCU with on-chip EtherCAT slave functions allows industrial application developers reduce their bill of materials (BOM) and support the miniaturization levels required for industrial equipment design.

"The RX72M Group offers revolutionary solutions for circuit board miniaturization, a key issue facing industrial robot designers as space constraints for boards continue to tighten," said Akira Denda, Vice President, Industrial Automation Business Division, Renesas Electronics Corporation. “Leveraging our extensive embedded design expertise as a leading global MCU supplier and solution provider for industrial networks, Renesas is pleased to introduce the RX72M devices, which allow approximately 50 percent reduction in circuit board area compared with earlier devices while maintaining high performance and EtherCAT support, offering customers an easy and flexible path to industrial equipment design."

The RX72M Group is the first RX MCU group to include an EtherCAT slave controller featuring the RX family’s highest SRAM capacity – 1 MB of SRAM – and 4 MB of Flash memory. The large-capacity SRAM allows the MCUs to run multiple memory-intensive middleware systems, such as TCP/IP, web servers, and file systems, at high speed without the use of external memory. It also provides flexibility for the support of future functional expansions, such as OPC United Architecture (OPC UA, Note 2) with no additional memory required. The on-board flash memory operates as two 2 MB banks, which enables stable operation of the end equipment, such as executing a program in one flash memory while simultaneously conducting background rewrites in the other flash memory.

Key features of the RX72M MCUs

  • The first EtherCAT slave controller for industrial Ethernet communication in an RX MCU
  • High performance with a CoreMark benchmark score of 1396 at up to 240 MHz, and the first embedded double precision floating point unit (FPU) in an RX MCU
  • High-speed flash memory system supporting readout up to 120 MHz, creating high-performance and low-variability execution environment
  • Dedicated trigonometric function (sin, cos, arctan and hypot functions) accelerators and register bank save function supporting high-precision motor control implementation – a feature shared with the Renesas RX72T motor-control MCUs
  • Reliable cryptography functions such as encryption module and memory protection function in hardware to protect encryption keys – this prevents application systems from being copied without authorization and supports authentication for genuine equipment
  • Flexible package options including 176-pin LQFP and 176-pin BGA configurations as well as the first 224-pin BGA package for RX MCUs, which offers additional space saving for size-constrained designs

Availability

Samples of the RX72M Group of MCUs are available now. Renesas will begin mass production orders starting September 2019. (Availability is subject to change without notice.)

More Information

To learn more about the new Renesas RX72M MCUs, visit https://www.renesas.com/products/microcontrollers-microprocessors/rx/rx700/rx72m.html

To learn more about Renesas’ industrial network solutions, visit https://www.renesas.com/solutions/industrial-automation/industrial-network/industrial-ethernet-and-fieldbus.html

Notes

Note 1: CoreMark: A benchmark test designed specifically for evaluating CPU core performance by the Embedded Microprocessor Benchmark Consortium (EEMBC®) of the United States. This test consists of a set of programs written in the C programming language that reads and writes data , integer operations and control calculations. The performance value per unit clock frequency is based on the CC-RX V3 C/C++ compiler for the RX family.

Note 2: OPC Unified Architecture (OPC UA) is an industrial communication data interchange standard.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) EtherCAT is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany. Coremark is a registered trademark of EEMBC. EEMBC is a registered trademark of the Embedded Microprocessor Benchmark Consortium. All registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.