QE for Capacitive Touch Feature - Two Types of Touch Judgment Modes with CTSU2 and QE
Oct 31, 2024
About This Video
You can select between two judgment modes—Value Majority Mode and Judgment Majority Mode—using QE for Capacitive Touch with a microcontroller equipped with CTSU2.
In developing embedded system using the capacitive touch sensor of MCUs, you can easily setup initial configurations of the touch interface as well as process the tuning of sensors, and reduce development time. [Plugin for Renesas IDE "e2 studio"] [Standalone Version] [Support MCU/MPU:RA, RL78, RX, Renesas Synergy™]