Skip to main content
Renesas Electronics Corporation

RX e² studio Project Tips - How To Convert an e² studio Sample Project Into a CS+ Project

RX e² studio Project Tips - How To Convert an e² studio Sample Project Into a CS+ Project
Jul 8, 2023

About This Video

This video explains how to convert a Renesas e² studio sample project into a CS+ project.

Transcript

Opening

This video explains how to convert a Renesas e² studio sample project into a CS+ project.

Introduction to project files (*.rcpc)

An e² studio CC-RX project can be converted into a CS+ project using a project file (*.rcpc) output by the e² studio export function. A project file (*.rcpc), which can be downloaded from the Renesas website, is already included in the e² studio sample program project.

Procedure for converting into CS+ project

Start CS+.
Display [Open Existing e² studio Project] from the [Start] tab.
Click [Go].

Select [Project File for e² studio (*.rcpc)] in the [Open Project] dialog.
Click [Open].

The [Project Convert Settings] dialog opens.
Select the project you want to convert from the Project list.
Select the device to use in [New microcontroller].
Set the project type, project name, and output destination of the converted project in [New project].
Click [OK] after completing all settings.

After the conversion is finished, the converted project will be opened.

About default debugger settings

After conversion, the default [Debug Tool] is [RX Simulator].

To change the debugger, select [RX Simulator (Debug Tool)] and right-click to open the menu.
Select the debugger to use from [Using Debug Tool].
For this video, the Debug Tool selected is [RX E2 Lite].

The selected Debug Tool has been changed to [RX E2 Lite (Debug Tool)].
If necessary, change the [Debug Tool] setting from each setting tab in [Property] tab.