Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Renesas Universal-TWT (U-TWT) Unleashed! Target Wake Time with No Strings Attached

Renesas Universal-TWT (U-TWT) Unleashed! Target Wake Time with No Strings Attached
May 14, 2026

About This Video

Building on the power management capabilities introduced with Wi-Fi 6, Target Wake Time (TWT) allows access points to schedule precisely when IoT devices wake up to access the wireless network — dramatically reducing power consumption for battery-operated devices. This webinar unpacks the fundamentals of Wi-Fi 6 TWT before diving into the Renesas DA16200's Universal-TWT feature, which breaks the dependency on Wi-Fi 6 infrastructure by bringing the same power-saving capabilities to non-Wi-Fi 6 access points and routers. Explore the key similarities between Universal-TWT and Wi-Fi 6 TWT, examine where Universal-TWT holds a distinct advantage, and understand why the DA16200 represents a compelling low-power solution for IoT designers looking to maximize battery life across a wide range of deployment environments.