Jun 23, 2018
About This Video
The RTOS configuration window is important if you use an RTOS with your project. The window carries many attributes for configuration and we will touch on these in the presentation. In this video we show you and briefly discuss the RTOS configuration window. Every ThreadX-based Synergy Project includes at least one RTOS Thread and a stack of SSP modules running in that thread. The Threads tab is a graphical user interface which helps you to add the right modules to a thread and configure the properties of both the threads and the modules associated with each thread. Once you have configured the thread, the ISDE automatically generates the code reflecting your configuration choices.