Skip to main content
Renesas Electronics Corporation

Renesas R-IN32M3 Industrial Ethernet Module: Multiprotocol IoT & Industry 4.0 Solution

Renesas R-IN32M3 Industrial Ethernet Module: Multiprotocol IoT & Industry 4.0 Solution
May 14, 2026

About This Video

Machine-to-machine communication underpins the automated processes at the heart of Industry 4.0 and IoT — and implementing the industrial Ethernet protocols that make it possible has historically been a significant development burden. This webinar introduces the Renesas R-IN32M3 Industrial Ethernet Module as a single solution that addresses three key requirements simultaneously: a low entry barrier through a multiprotocol approach with all licenses included, straightforward implementation with a clear migration path to Renesas ASSP devices via a dual-port RJ45 form factor, and fast time to market backed by a solution kit, software package, and certifications. A practical session for industrial automation designers looking to reduce the complexity of industrial Ethernet integration.