Overview
The YRPBRL78G13 is a promotion board for the Renesas RL78 microcontroller family. It supports on-board debugging, flash programming, and is pre-programmed to work with the GUI provided on the included DVD to demonstrate the low-power capabilities of the Renesas RL78 MCU.
Features
- Easy to use device demonstration capabilities
- Power supply via USB interface
- On-board debug function by using the IAR CSPY debugger
- WriteEZ5 Flash programming software (preliminary version)
- Applilet3 Device driver code generator (preliminary version)
- Various input/output signals available, such as all I/O ports, virtual UART interface and 1 LED
- Included IAR Embedded Workbench for RL78 and the IAR C-SPY debugger
Sample & Buy
YRPBRL78G13-RL78/G13
ActiveVideos & Training
Additional Videos
Support
Support Communities
- YRPBRL78G13 Stick - Programming FLASH has no effect
Greetings RenesasRulz Forum, Looks like my first post is going to be one of the most basic: I have been compiling a simple blinky light for the YRPBRL78G13 Stick demo. The light is located at P77. I have attached my code/project to this post. The issue I am ...
May 11, 2015 - YRPBRL78G13_Stick_Demo_SW.hex
YRPBRL78G13_Stick_Demo_SW.hex (MCU - R5F109AEx) Please verify the Schematic and Provide any Corrections/Suggestions if any to improve the circuit. Thanks in advance. (MCU - R5F109AEx) Please verify the Schematic and Provide any Corrections/Suggestions if any to improve the circuit. Thanks in advance.
- YRPBRL78G13_Stick_Demo_SW.hex
YRPBRL78G13_Stick_Demo_SW.hexHi Team, Iam working on R5F109AEx MCU to generate A PWM signals for Automotive LED Animation. For Communication protocol is LIN. I have an Doubt for ADC configuration. I need the ADC configuration. can you please verify the circuit.Hi Team, Iam working on R5F109AEx MCU ...