Skip to main content
Renesas Electronics Corporation

Overview

The SLG46625AP-SKT GreenPAK™ 35x35 socket adapter kit enables users to configure, program, and test the SLG46625-A automotive GreenPAK programmable mixed-signal matrix using the SLG4DVKADV GreenPAK Advanced Development Board or SLG4DVKLITE GreenPAK Lite Development Board. The SLG46625AP-SKT kit includes the SLG4SA20-35x35 socket adapter and 50 SLG46625-AP samples.

The SLG46625-A IC is installed into the TQFN-20 socket on the socket adapter, which then connects to the socket connector on the Advanced Development Board. The Advanced Development Board can then be connected to a PC running the GreenPAK Designer software.

Features

  • TQFN-20 socket for SLG46625-A Automotive GreenPAK Mixed-Signal Matrix
  • SLG4SA20-35x35 socket adapter
  • 50 SLG46625-AP IC samples

Products in the Design

Sample & Buy

SLG46625AP-SKT Socket Adapter Kit

SLG46625AP-SKT

Active
Pb (Lead) Free:Yes
ECCN (US):EAR99
HTS (US):8473.30.1180
1u | $60.00Budgetary Price

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

GreenPAK Advanced Development Board

SLG4DVKADV Active
Serve as the core platform for programming, emulation, and in-circuit testing across the GreenPAK programmable mixed-signal portfolio.

GreenPAK Lite Development Board

SLG4DVKLITE Active
Program, emulate, and test GreenPAK devices using a streamlined development board integrated with Go Configure software.

Go Configure Development Board

Program, emulate, and prototype ForgeFPGA and GreenPAK designs using a universal development board tightly integrated with the Go Configure Software Hub.

GreenPAK Extension Card for the Go Configure Development Board

SLG4EXTCARD1 Active
The GreenPAK™ Extension Card #1 is designed to work with the Go Configure Development Board, providing a platform for evaluating, debugging, and validating GreenPAK mixed-signal ICs. This extension card is required to connect to and use the GreenPAK socket adapters and DIP adapters.