Overview
Description
The SLG46620V-SKT is a socket adapter kit for use with the SLG4DVKADV GreenPAK™ Advanced Development Board or SLG4DVKLITE GreenPAK Lite Development Board. The SLG46620V-SKT includes the SLG4SA20-20x30 socket adapter and 50 SLG46620V (STQFN-20) GreenPAK programmable mixed-signal matrix IC samples.
Used with SLG46xxxX-SKT and SLG47xxxV-SKT socket kits, the GreenPAK Advanced and Lite Development Boards provide full programming, emulation, and testing functions for GreenPAK devices.
The SLG46620 provides a small, low-power component for commonly used mixed-signal functions. The user creates their circuit design by programming the one-time programmable (OTP) non-volatile memory (NVM) to configure the interconnect logic, the I/O pins, and the macrocells of the SLG46620.
Features
- STQFN-20 socket for the SLG46620 GreenPAK programmable mixed-signal matrix
- SLG4SA20-20x30 socket adapter
- 50 SLG46620V IC samples
Applications
Design & Development
Videos & Training
Additional Videos
Support
Support Communities
- SLG46620V board and socket
Hello Dear I would like to buy the SLG46620V model. My question is, the board and socket to work with it could be the same that that used with the board SLG4DVKADV. It is because I have that board for another chip ( SLG46826V-SKT) and I dont know if I ...
Jan 8, 2020 - Debuggin controls
Hello I am trying to do simulations using the packet SLG46620V-SKT and the mode advance development plataform (attach pdf). Is it possible to obtain plots using that platform . Thank you very much Regards Daniel
Oct 29, 2020