Skip to main content
Renesas Electronics Corporation

Description

The Renesas Starter Kit for RL78/G1C is intended as a user-friendly introductory and evaluation tool for the RL78/G1C microcontroller. The board provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging using CubeSuite+.

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run, only minutes after opening the box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Note: CubeSuite+ is not generally promoted to the U.S. and European customers. Customers in the U.S. and Europe ,who are interested in CubeSuite+, are requested to contact our regional marketing departments for details.

Features

  • Renesas microcontroller programming
  • User code debugging
  • User circuitry such as switches, LEDs, and a potentiometer
  • Sample application
  • Sample peripheral device initialization code

Applications

Type Title Date
Manual - Development Tools PDF 217 KB
Tool News - Release PDF 261 KB 日本語
Tool News - Notification PDF 153 KB 日本語
PCB Design Files
Log in to Download ZIP 1.01 MB 日本語
Application Note PDF 1.31 MB 日本語
AI-generated Summary: The document defines key terms and abbreviations related to Renesas USB Peripheral Communications Device Class Driver (PCDC), explaining the roles of API, APL, CDC, PCD, and other components. It describes how to register a class driver with BASIC-FW using usb_papl_registration(). The operating environment includes specific compilers and evaluation boards. Software configuration details the module structure, highlighting interactions between user application (APL), PCDC, PCD, and CPD, with tasks managed by a scheduler to prioritize operations and enable non-blocking communication.
Application Note PDF 1.07 MB 日本語
AI-generated Summary: The document details the Renesas USB MCU USB Peripheral Mass Storage Class Driver (PMSC) architecture and operating environment. It defines key terms and abbreviations related to USB mass storage communication, including APIs and driver layers. The software configuration includes a layered structure with PDCD composed of PMSCD and PMSDD, where PMSCD manages BOT protocol communication and PMSDD handles storage commands and media access. The operating environment specifies compatible compilers and evaluation boards used for confirmation.
Application Note PDF 1.07 MB 日本語
AI-generated Summary: This document details the Renesas USB MCU USB Host Android Open Accessory (AOA) software, including terms, abbreviations, and how to use the document. It explains registering device class drivers, compliance with Android Open Accessory specifications (versions 1.0 and 2.0), and basic AOA functions such as device verification and data transfer. The operating environment includes specific compilers and evaluation boards. The software configuration covers module components like user applications, vendor class drivers, and USB host control drivers, describing their roles and interactions.
Application Note PDF 1.30 MB 日本語
AI-generated Summary: This document defines terms and abbreviations related to Renesas USB Host Communication Device Class Driver (HCDC) and explains how to register the class driver with USB-BASIC-F/W. It details the operating environment, including supported compilers and evaluation boards. The software configuration section describes the module structure, highlighting the user application (APL), HCDC driver, and USB-BASIC-F/W firmware. The host demo application sets serial communication parameters, echoes received data, and allows baud rate changes via user switches on the evaluation board.
Application Note PDF 1.36 MB 日本語
AI-generated Summary: The document explains the structure and operation of the USB Host Human Interface Device Class Driver (HHID) for Renesas USB MCUs. It details how to register the class driver with USB-BASIC-F/W, the supported compilers and evaluation boards, and the software module configuration including user application, HHID, and USB-BASIC-F/W. The host demo application functions include receiving data from USB mouse and keyboard devices, displaying information on an LCD, handling suspend/resume states, and controlling LEDs based on device input and state changes.
Application Note PDF 2.08 MB 日本語
AI-generated Summary: The USB-BASIC-F/W firmware simplifies USB communication development for Renesas USB MCUs by providing sample source code for hardware control, supporting both host and peripheral modes at full and low speeds. It uses a task-based scheduler with non-blocking callbacks to prioritize functions. Users register class drivers for host or peripheral modes via specific functions. The firmware offers APIs for control, bulk, and interrupt transfers, remote wakeup, and supports multiple data transfers on the same pipe. Sample applications demonstrate enumeration and data transfer operations.
Application Note PDF 1.50 MB 日本語
AI-generated Summary: This document defines terms and abbreviations related to Renesas USB MCU Peripheral Human Interface Devices (PHID) class driver and explains how to read the document. It details the registration process of the PHID class driver with USB-BASIC-FW and lists supported compilers and evaluation boards used for operation confirmation. The software configuration section describes the modular structure of PHID, including hardware drivers, USB peripheral control, and user application, highlighting the communication flow between user switches, HID reports, and USB-BASIC-FW.
Application Note PDF 533 KB
AI-generated Summary: The document explains how to open and manage sample projects in CubeSuite+ for the RL78/G1C Renesas Starter Kit. It guides users to open the tutorial project file, navigate the Project Tree to access source and dependent files, and set active projects. Each sample project contains C source files generated by the Application Leading Tool, demonstrating peripheral initialization and functionality. An example ADC project shows how to perform A/D conversions triggered by switch presses, displaying results on an LCD and allowing user interaction with a potentiometer.
Application Note PDF 426 KB
AI-generated Summary: The document explains how to import sample projects for the RL78/G1C Renesas Starter Kit into the e2studio IDE. It guides users to start e2studio, open the Import dialog, select 'Existing Projects into Workspace' under the General folder, and browse to the project directory. Users must ensure the option to copy projects into the workspace is selected before finishing the import. The projects include various examples like ADC, Async Serial, DMAC, and Low Power Mode.
Manual - Development Tools PDF 758 KB
Manual - Development Tools PDF 1.67 MB
Quick Start Guide PDF 106 KB
Manual - Development Tools PDF 155 KB 日本語
Manual - Development Tools PDF 836 KB 日本語
Manual - Development Tools PDF 1.68 MB 日本語
19 items

Software & Tools

Software & Tools

Software title
Software type
Company
CS+
Renesas integrated development environment (IDE) [Support MCU/MPU: RH850, V850, RX, RL78, 78K0R, 78K0] (Note: CS+ is not generally promoted to U.S. and European customers.) (Note: To use Smart Configurator on CS+ for RL78/G23 and RX family MCUs, install the Smart Configurator for each MCU family separately downloading from ”Design & Support” > ”Development Tools” > ”Smart Configurator”)
IDE and Coding Tool Renesas
Renesas Flash Programmer (Programming GUI)
Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, RISC-V MCU, Renesas Synergy, DA1453x, DA1459x, DA1469x, DA1470x, DA148xx, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78K0R, 78K0]
Programmer (Unit/SW) Renesas
2 items

Software Downloads

Type Title Date
Software & Tools - Other
Log in to Download ZIP 696.49 MB
Software & Tools - Other
Log in to Download ZIP 736.57 MB
2 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 8.16 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 5.71 MB 日本語 Compiler: NC30WA IDE: HEW
Sample Code
Log in to Download ZIP 5.51 MB 日本語 Compiler: CA78K0R, CC-RL IDE: CS+, e2 studio
Sample Code
Log in to Download ZIP 6.60 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 6.73 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 5.38 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 8.47 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 8.06 MB 日本語 Compiler: CA78K0R, CC-RL, ICCRL78, KPITGCC, NC30WA IDE: CS+, e2 studio, HEW, IAR EWRL78
Sample Code
Log in to Download ZIP 2.88 MB IDE: e2 studio
9 items
Part NumberStatusStockBudgetary Price (USD)DescriptionDebugger supplied
R0K5010JGS900BEActiveIn Stock1u | $258.82Renesas Starter Kit for RL78/G1C (Kit with CubeSuite+)None
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
Icon showing CD-ROM illustration, indicating compact disc storage.

ROM Ordering

Embed your custom code into Renesas masked MCUs during manufacturing for tailored device functionality.