Skip to main content
Renesas Electronics Corporation

Overview

DA14580PRODTLKT is not recommended for new designs. The recommended alternative is the Connectivity Production Line Tool.

Renesas offers a production test and programming unit that enables you to reduce the time to ramp-up at a lower cost. The SmartBond Production Line Tool (PLT) helps to increase throughput in volume test and programming of units centered around the Renesas Bluetooth® ICs.

We work with a number of 3rd parties and distributors globally to support this platform. Contact your local Renesas sales office if you would like more information on how Renesas can support your volume production test and programming.

The release of the SmartBond Production Line Tool supports devices in the SmartBond™ Bluetooth families: DA1453x, DA1459x, DA1469x, and DA1470x.

Features

  • Ease of integration: DLL based commands
  • Flexibility in programming OTP/Flash/EEPROM
  • Low overall cost of tester equipment
  • High level of parallelization and short testing time
  • Up to 16 times parallel programming and test

Sample & Buy

DA14580PRODTLKT Production Line Tool Kit Board

DA14580PRODTLKT

Not Recommended for New Designs
MOQ:1
SPQ:1
Pb (Lead) Free:Yes
Carrier Type:Box
Assembly Location:GERMANY
1u | $1,100.00Budgetary Price

Support

Support Communities

  1. DA14531 for mass production programming

    Hello team renesas, I want to know the process of programming DA14531 in mass production. Here we want to store our firmware in SPI flash not in OTP so we can preform SUOTA. So how can i perform this and also guide what changes should i do in firmware before ...

    Nov 21, 2022
  2. cli_programmer not working under Windows 11

    Hi, after upgrading my operating system from Windows 10 to 11, the cli programmer no longer works in SmartSnippets Studio. There is another Thread on here discussing the same issue, but I was asked to start a new one. I am using SmartSnippets Studio 1.6.3, as this is ...

    Oct 30, 2024
  3. DA14531-00 is not advertising if I come out of the debug mode in keil ide. why?

    Hi,    I'm using DA14531-00FXDEVKT-P. I downloaded Keil ide and SDKs. I'm using Ble examples in "SDK\DA145xx_SDK\6.0.22.1401\projects\target_apps\ble_examples". if I run the code in debug mode in keil ide then DA14531 is advertising. but if I come ...

    Jun 18, 2024
View All Results from Support Communities (23)