Overview
DA14580PRODTLKT is not recommended for new designs. The recommended alternative is the Connectivity Production Line Tool.
Renesas offers a production test and programming unit that enables you to reduce the time to ramp-up at a lower cost. The SmartBond Production Line Tool (PLT) helps to increase throughput in volume test and programming of units centered around the Renesas Bluetooth® ICs.
We work with a number of 3rd parties and distributors globally to support this platform. Contact your local Renesas sales office if you would like more information on how Renesas can support your volume production test and programming.
The release of the SmartBond Production Line Tool supports devices in the SmartBond™ Bluetooth families: DA1453x, DA1459x, DA1469x, and DA1470x.
Features
- Ease of integration: DLL based commands
- Flexibility in programming OTP/Flash/EEPROM
- Low overall cost of tester equipment
- High level of parallelization and short testing time
- Up to 16 times parallel programming and test
Sample & Buy
DA14580PRODTLKT
Not Recommended for New Designs| MOQ: | 1 |
| SPQ: | 1 |
| Pb (Lead) Free: | Yes |
| Carrier Type: | Box |
| Assembly Location: | GERMANY |
Resources
Support
Support Communities
- ERROR ---Failed to close COM port in DA14531MOD module at the time of firmware update
Hi Renesas Team, Actually i was trying to load code in da14531mod but it stuck after reset button detected at ERROR Booter@25-10-17 12:29:37] Failed to close COM6 can u please help how to resolve these is what is the reason of these [INFO Flash Code ...
Oct 17, 2025 - DA14680 J-Flash configuration missing
Hi Folks, we have to bringup a rather old project in which a DA14680 is used. According to the documentation, the recommendation to flash the device is by using the SEGGER J-Link / J-Flash toolchain (is this correct?). Using J-Flash the DA14680 could be selected, but there ...
May 11, 2023 - Intermittent issues while programming DA14531 using PRO Development kit via JTAG
While trying to program DA14531 using the JTAG method via the PRO Development board, the ERASE/PROGRAM fails intermittently (with a success rate of about 75%). The software used for programming is Dialog SmartBond Flash Programmer v1.0.8.3896. We followed the same connection as mentioned in the ...
Jan 31, 2023