Skip to main content
Renesas Electronics Corporation

Renesas Blog

SW platform and dev. env. for E/E architecture series 1; Solution Project of Automotive Development Environment

SW platform and dev. env. for E/E architecture series 1; Solution Project of Automotive Development Environment

Nowadays, software has become the core of the value of the car. We are proposing and developing a development environment that contributes to the development of such software-centric cars.

200/400/800Gbps Fixed Form Factor Switch Solution Blog

Solving Synchronization and Clock Jitter Challenges with ClockMatrix™ 2 for 400Gbps+ Pizza Box Network Switches

The ultra-low jitter ClockMatrix 2 eliminates the need for additional jitter attenuators for high-speed interfaces and supports multiple standards and protocols including Sync-E and IEEE 1588.

Water level measurement solution blog

Realizing a Low-Cost Water Level Measurement Solution Using the RX130’s Capacitive Touch Key

Introducing a reference design demo that can measure the amount of remaining liquid with the RX130 MCU, using its built-in Capacitive Touch Sensor Unit (CTSU) and copper electrodes.

Blog image Secure Boot

Achieving a Root of Trust with Secure Boot in Automotive RH850 and R-Car Devices – Part 1

This article is the first in a series of three blog articles introducing the reader to secure boot concepts and implementations in Renesas automotive devices.

Use the Latest Technology in Your Next BLDC Motor Control Design

Use the Latest Technology in Your Next BLDC Motor Control Design

Learn about Renesas’ BLDC Traction Motor Drive solution that is built around two dedicated motor control devices for the perfect combination of processing speed and power efficiency.

Heat Suppression & Loss Reduction! Solution for Li-ion Battery – Industrial Power MOSFET

Renesas’ “Shunt-less solution” can be realized by a power MOSFET with current detecting function in combination with a Battery Management IC (BMIC).
The Art of Networking: MACsec and CANsec – Layer 2 Security for High Performance Networks

The Art of Networking (Series 6): MACsec and CANsec – Layer 2 Security for High Performance Networks

In this blog, we will explain security acceleration methods that are being standardized for CAN and Ethernet to improve the security performance and offload tasks to hardware.

Seamlessly Switch to a 32-Bit RX Family MCU

To Seamlessly Switch to a 32-Bit RX Family MCU

Renesas has prepared a “Migration Guide” and “Points of Differences” to support replacement from Renesas legacy MCU products to the RX 32-bit MCU family, as well as between the RX family itself.

Achieve Ultra-Lower Designs Using the RA2E1 MCU and Flexible Software Package (FSP).

Achieve Ultra-Lower Designs Using the RA2E1 MCU and FSP

Quickly develop a low power data logger application on the RA2E1 32-bit MCU using its “Snooze” mode for significant power savings, Flexible Software Package (FSP) and Fast Prototyping Board (FPB).

Address the challenges of network-connected equipment by using 32-bit RX66N MCUs.

Would You Like to Address the Challenges of Network-Connected Equipment by Using 32-Bit RX66N MCUs?

Introducing the RX66N 32-bit MCU that realizes real-time performance and firmware updates required for network-connected equipment such as smart meters and HVAC controllers.