Inductive Position Sensor IPS2550, The Ideal xEV Position Sensor for Resolver Replacement
Are you looking for the best position sensor for your xEV motor? We will introduce the IPS2550 inductive position sensor and our inverter system using it.
Are you looking for the best position sensor for your xEV motor? We will introduce the IPS2550 inductive position sensor and our inverter system using it.
This blog describes trends, challenges and solutions for battery management systems facing an increasing number of battery cells.
As machine learning (ML) inference moves to device endpoints, integrated AI will power a complex combination of tech to create smart applications with which we can interact more naturally.
Hidetoshi Shibata, Renesas’ CEO, recently joined the FT Global Dealmaking Summit 2021 hosted by the Financial Times and shared Renesas’ M&A goals and recent examples.
The 32-bit RX family MCU enables application development with less or no coding. This blog is about our support for development of small and low-power embedded devices with internet connection.
A force sensor can be mounted to the tip of a robotic arm to measure load and torque. This blog introduces the Application Note on force sensing measurement using the RX23E-A 32-bit MCU.
CASE+Eのこれからの自動車業界において半導体
に求められる価値提供、及び当社のアプローチをご紹介します。
This blog helps customers find the right devices to use when they are looking for a high-performance clock to drive their data converters.
The Qwicc Wi-Fi Shield based on Renesas’ Wi-Fi DA16200 module, is an Arduino Uno R3 form factor shield that enables rapid development of ultra-low power Wi-Fi IoT applications.
Renesas' DA16200 Wi-Fi System-on-Chip (SoC) and modules have won the Communication Technology category at Elecfans' annual China IoT Innovation Awards.