Skip to main content
Renesas Electronics Corporation

Renesas Blog

NFC Revolutionizing IoT Applications: A Seamless Future Blog

NFC Revolutionizing IoT Applications: A Seamless Future

Embrace the future of connectivity and enhance your application with Renesas' PTX105R NFC controller for Internet of Things applications, the most suitable NFC reader on the market.

Renesas QEMU Environment is a simulator for R-Car S4 that achieves high-speed simulation

High-Speed Simulator for R-Car S4 - Renesas QEMU Environment

Introducing a high-speed simulator for R-Car S4, the Renesas QEMU Environment.

AI Coding with ChatGPT for RL78 Microcontrollers (Arduino)

AI Coding with ChatGPT for RL78 Microcontrollers (Arduino)

In this blog introduces how to do AI coding using ChatGPT and the RL78 Arduino-compatible board, along with its practical examples.

 The IoT Cloud Connection Decision: Wi-Fi or Cellular?

The IoT Cloud Connection Decision: Wi-Fi or Cellular?

With the ubiquity of wireless connectivity options on IoT devices, connection to the cloud has become more flexible than ever. Traditionally, Wi-Fi has been the most popular choice in the IoT world although this has changed in recent years with the huge strides made in cellular networks. However, there is no right answer for which option would be the best or the more efficient between the two.

The type of network connection to use depends on several factors that affect solution development.

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

The AIoT has been enabled by higher MCU compute capability and thin neural network models that are more suited for edge and end point devices than traditional CPUs and MPUs.

Renesas Initiatives in Smart Agriculture - Part 1

Renesas Initiatives in Smart Agriculture - Part 1

Introduction to Renesas solutions for smart agriculture

Closing the Performance Gap Between DRAM and AI Processors

Closing the Performance Gap Between DRAM and AI Processors

Blog discussing Renesas’ memory interface solutions

Let's Create a Digital Angle Meter Using a Microcontroller

Let's Create a Digital Angle Meter Using a Microcontroller

We’ll create a digital angle meter using the RL78/G15 Fast Prototyping Board. The data from the gyro sensor will be converted into angles and displayed on the LCD.

Introducing An Easy Tool for Touch Development Even with Partner IDE Platforms

Introducing An Easy Tool for Touch Development Even with Partner IDE Platforms

By using the standalone version of QE for Capacitive Touch, you can develop capacitive touch applications even with IAR's EWRX IDE.

Real-time Vision AI Runs at the Size of a Raspberry Pi! Introducing the RZBoard V2L Single Board Computer

Real-time Vision AI Runs at the Size of a Raspberry Pi! Introducing the RZBoard V2L Single Board Computer

Introducing the RZBoard V2L, a small single-board computer that enables easy Vision-AI trial with the RZ/V2L MPU.