TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced its full commitment to meet the ISO/SAE 21434 road vehicles cybersecurity engineering international standard for its automotive microcontrollers (MCUs) and system on chip (SoC) solutions effective with new developments from January 2022. This is part of the company’s continued commitment to implement robust automotive cybersecurity management systems (CSMS) as part of the new UN Economic Commission for Europe (UNECE) regulation UN R155.
The commitment reaffirms to original equipment manufacturers (OEMs) and Tier1 suppliers that Renesas will continue to meet its CSMS responsibilities. All future Renesas automotive MCUs and SoCs will sequentially follow the ISO/SAE 21434 standard with development starting from January 2022. This includes the company’s 16-bit RL78 and 32-bit RH850 MCUs as well as Renesas’ popular R-Car SoC Family.
Both ISO/SAE 21434 (released on August 31, 2021) and UNECE UN R155 require cybersecurity to be enforced across the entire automotive supply chain. Effective July 2022, for new vehicle types, automotive OEMs will be required to have an automotive CSMS in place to ensure that the stringent cybersecurity processes have been implemented to gain vehicle type approval. With Renesas’ commitment to ISO/SAE 21434, OEMs and Tier1 suppliers can have confidence in adopting Renesas’ solutions.
“ISO/SAE 21434 is setting the international standard that outlines the requirements for security throughout the entire automotive life cycle, and Renesas has now adopted this standard. We will establish security process with requirement definition by security analysis, implementation and evaluation, utilizing and optimizing existing development process.” said Takashi Yasumasu, Vice President of Automotive Core Technology Development Division at Renesas. “This enables us to provide products and solutions with appropriate risk mitigation measures according to the risk assessment. Renesas aims to be a trusted partner for customers around the world in the face of the growing automotive security threats posed by CASE.”
Renesas has made significant global contributions to the development of the ISO/SAE 21434 standard. In 2019, Renesas was certified by TÜV Rheinland as compliant with the IEC 62443-4-1 standard, which specifies the requirements for security development process of industrial products.
While leveraging these achievements and experiences, Renesas will continue to upgrade its automotive CSMS process to address new requirements and expectations called out in ISO/SAE 21434 and enhance its effective cybersecurity measures. Renesas' automotive CSMS will assign not only leaders responsible for hardware and software security development, but also system security leaders to address system use cases, aiming to provide not only compliance with standards but also optimal solutions. Renesas will continue to contribute to the development of safe and secure products for our customers. continuing its long history of developing MCU and SoC which comply with ISO 26262, Renesas commits to meet additionally cybersecurity market needs including ISO/SAE 21434 requirements.
For more information, please visit: https://www.renesas.com/application/automotive/automotive-security
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.