Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Renesas Introduces 64-bit RZ/G3E MPU for High-Performance HMI Systems Requiring AI Acceleration and Edge Computing

MPU Integrates a Quad-Core CPU, an NPU, High-Speed Connectivity and Advanced Graphics to Power Next-Generation HMI Devices with Full HD Display

July 29, 2025

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the launch of its new 64-bit RZ/G3E microprocessor (MPU), a general-purpose device optimized for high-performance Human Machine Interface (HMI) applications. Combining a quad-core Arm® Cortex®-A55 running at up to 1.8GHz with a Neural Processing Unit (NPU), the RZ/G3E brings high-performance edge computing with AI inference for faster, more efficient local processing. With Full HD graphics support and high-speed connectivity, the MPU targets HMI systems for industrial and consumer segments including factory equipment, medical monitors, retail terminals and building automation.

High-Performance Edge Computing and HMI Capabilities

At the heart of the RZ/G3E is a quad-core Arm Cortex-A55, a Cortex-M33 core, and the Ethos™-U55 NPU for AI tasks. This architecture efficiently runs AI applications such as image classification, object recognition, voice recognition and anomaly detection while minimizing CPU load. Designed for HMI applications, it delivers smooth Full HD (1920x1080) video at 60fps on two independent displays, with output interfaces including LVDS (dual-link), MIPI-DSI, and parallel RGB. A MIPI-CSI camera interface is also available for video input and sensing applications.

“The RZ/G3E builds on the proven performance of the RZ/G series with the addition of an NPU to support AI processing,” said Daryl Khoo, Vice President of Embedded Processing at Renesas. “By using the same Ethos-U55 NPU as our recently announced RA8P1 microcontroller, we’re expanding our AI embedded processor portfolio and offering a scalable path forward for AI development. These advancements address the demands of next-generation HMI applications across vision, voice and real-time analytics with powerful AI capabilities.”

The RZ/G3E is equipped with a range of high-speed communication interfaces essential for edge devices. These include PCI Express 3.0 (2 lanes) for up to 8Gbps, USB 3.2 Gen2 for fast 10Gbps data transfer, and dual-channel Gigabit Ethernet for seamless connectivity with cloud services, storage, and 5G modules.

Low-Power Standby with Fast Linux Resume

Starting with the third-generation RZ/G3S, the RZ/G series includes advanced power management features to significantly reduce standby power. The RZ/G3E maintains sub-CPU operation and peripheral functions while achieving low power consumption around 50mW and around 1mW in deep standby mode. It supports DDR self-refresh mode to retain memory data, enabling quick wake-up from deep standby for running Linux applications.

Comprehensive Linux Software Support

Renesas continues to offer the Verified Linux Package (VLP) based on the reliable Civil Infrastructure Platform, with over 10 years of maintenance support. For users requiring the latest versions, Renesas provides Linux BSP Plus, including support for the latest LTS Linux kernel and Yocto. Ubuntu by Canonical and Debian open-source OS are also available for server or desktop Linux environments.

Key Features of RZ/G3E

  • CPU: Quad-core Cortex-A55 (up to 1.8GHz), Cortex-M33
  • NPU: Ethos-U55 (512 GOPS)
  • HMI: Dual Full HD output, MIPI-DSI / Dual-link LVDS / Parallel RGB, 3D graphics, H.264/H.265 codec
  • Memory Interface: 32-bit LPDDR4/LPDDR4X with ECC
  • Connectivity for 5G Communication: PCIe 3.0 (2 lanes), USB 3.2 Gen2, USB 2.0 x2, Gigabit Ethernet x2, CAN-FD
  • Operating Temperature: -40°C to 125°C
  • Package Options: 15mm square 529-pin FCBGA, 21mm square 625-pin FCBGA
  • Product Longevity: 15-year supply under Product Longevity Program (PLP)

System-on-Module Solutions from Renesas and Ecosystem Partners

Renesas has also introduced system-on-module (SoM) solutions featuring the RZ/G3E. A broad range of SoM solutions will be available from Renesas’ ecosystem partners such as a SMARC module from Tria, an OSM (Size-M) from ARIES Embedded, and an OSM (Size-L) from MXT.

Winning Combinations

Renesas combined the RZ/G3E with other compatible devices to develop Full HD Dual-Display HMI Platform and Digital Otoscope solutions. These Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly. They can be found at renesas.com/win.

Availability

The RZ/G3E is available today, along with the Evaluation Board Kit. The kit includes a SMARC v2.1.1 module board and a carrier board. More information about Renesas RZ/G3E is available at: https://www.renesas.com/rzg3e

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.