Skip to main content
Renesas Electronics Corporation

Renesas Unveils Automotive Gateway Solution Based on New R-Car S4 SoCs and PMICs for Next-Generation Vehicle Computers

Highly Integrated R-Car S4 Accelerates Centralization with High Performance, Networking, Security and Safety Features , basic_html

October 6, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today unveiled an innovative automotive gateway solution with R-Car S4 system on chips (SoCs) and power management ICs (PMICs) for next-generation vehicle computers, communication gateways, domain servers and application servers. Renesas' new solution meets the automotive industry's high demands for high performance, high-speed networking, high security and high functional safety levels that are required as E/E architectures evolve into domains and zones. The solution also dramatically improves development efficiency by enabling software reusability and including the new best-in-class PMICs designed to work seamlessly with the R-Car S4.

“As the vehicle architectures evolve, safe connection to cloud services and secure management with in-vehicle control systems are major challenges,” said Takeshi Kataoka, Senior Vice President and General Manager of Automotive Solution Business Unit at Renesas. “As an automotive market leader, we have addressed these challenges with our new R-Car S4 solution, and global OEMs have already begun to design next-generation systems with this solution.”

The Renesas R-Car S4 is one of the first products in Renesas’ 4th-generation R-Car Family. It includes multiple Arm® Cortex® A55, Cortex R52 and is the first to implement an RH850 MCU for control domain management. R-Car S4 SoCs offer a huge number of automotive interfaces such as 16x CAN FD, 16x LIN, 8x SENT, 1x FlexRay, 4x PCIe V4.0 and also a high-bandwidth 3 x 2.5Gbit Ethernet Switch to enable rich communication and connectivity options both inside and outside of the vehicle.

The R-Car S4 solution allows designers to re-use up to 88 percent of software code developed for 3rd generation R-Car SoC and RH850 MCU applications. The software package supports R-Car S4 application development including the real-time cores with various drivers and basic software such as Linux BSP and hypervisors. In addition, a virtual platform (VPF) is available from a partner company, enabling early software development and evaluation to reduce design time and cost.

The new PMICs for R-Car provide advanced power modes that support extremely low power operation. The RAA271041 PMIC accepts the vehicle’s 12V supply and supports wide operation for load dump and cold cranking pulses while providing the first-stage regulation. The RAA271005 is a Safe 11-channel PMIC that takes the RAA271041’s output and steps it down further to the various supply voltages needed by R-Car S4 and its peripherals such as LPDDR4x memory. The RAA271041 and RAA271005 PMICs provide a complete power solution from vehicle battery down to system voltage.

Renesas will provide the evaluation boards as a Winning Combination solution featuring the R-Car S4 device, the RAA271041 and RAA271005 PMICs, and a Renesas timing IC (Autoclock RC2121x). This pre-tested solution will reduce risk in the board design and will further shorten the development cycle.

Key Features of the R-Car S4 SoCs

  • Eight 1.2 GHz Cortex A55 cores, one 1.0 GHz Cortex® R52 dual core (lock-step) and two 400 MHz RH850 G4MH dual cores (lock-step) deliver up to 27 KDMIPS application performance plus greater than 5.3 K DMIPS real-time performance
  • Abundant automotive interfaces including 16x CAN FD, 16x LIN, 8x SENT, 1x FlexRay, and 4x PCIe V4.0 allow a wide range of connectivity inside the vehicle
  • Integrated Ethernet TSN switch offers bandwidth of 3 x 2.5 Gbps to deliver fast and low-latency communication in the vehicle backbone and to the outside world. This switch is fully validated by Spirent’s TSN conformance test solutions running on their Automotive C1 test system.
  • Incorporated 8MB SRAM to execute code on the RH850 G4MH core with low latency
  • Multiple hardware security modules (HSMs) provide enhanced security protection against cyber attacks
  • R-Car S4 is compliant to ISO-26262 and supports functional safety according to ASIL B and ASIL D
  • 23mm square (R-Car S4) and 19mm square (R-Car S4N) FCBGA packages

Key Features of the PMICs for R-Car

  • Programmability enables easy adaption to support R-Car S4 and future R-Car SOCs
  • RAA271041 and RAA271005 provide advanced power control to support extremely low power operation for always-on, DeepSTOP, cyclic-run, and suspend-to-ram modes.
  • RAA271041 is a pre-regulator that offers two 42V synchronous controllers, one buck and one boost. The device’s boost stage supports the buck stage when the battery voltage drops during cranking transients as low as 2.5V.
  • RAA271041 and RAA271005 were developed per ISO-26262 and are capable of supporting system safety requirements up to ASIL D.
  • Integrated 12-bit SAR ADC monitors external signals and eliminates an external ADC
  • Dynamic Voltage Frequency Scaling changes output voltage to save power
  • Optional spread-spectrum clocking mitigates EMI
  • Built-in support for R-Car S4 activation streamlines SoC self-test procedures

Availability

Samples of the R-Car S4 SoCs and evaluation boards are available now. For more information, please visit:
https://www.renesas.com/products/automotive-products/automotive-system-chips-socs/r-car-s4-automotive-system-chip-soc-car-servercommunication-gateway.

Samples of the RAA271041 and RAA271005 are available now. More information is available at https://www.renesas.com/RAA271041 and https://www.renesas.com/RAA271005.

For more information on Renesas automotive gateway solution, go to https://www.renesas.com/application/automotive/automotive-communication-gateway-platform.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.

(Remarks). Arm and Arm Cortex are registered trademarks of Arm Limited in the EU and other countries. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.