メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation) - 6月はプライド月間として、LGBTQ+の権利や文化、コミュニティについて啓発する世界的な活動月間です

DA16600 Enables Matter Over Wi-Fi

DA16600 Enables Matter Over Wi-Fi
2024年3月2日

このビデオについて

Explore the seamless integration of smart home devices using Renesas' DA16600 module, which incorporates a DA16200 Wi-Fi SoC and a DA14531 Bluetooth Low Energy SoC. In this demonstration, the DA16600 sensor module is showcased alongside Amazon Echo Dot and Google Nest Mini smart home hubs, connected via Wi-Fi 6 technology for enhanced capacity and connectivity. Utilizing Matter's Multi-hub feature, users can control smart lighting effortlessly, toggling between hubs with voice commands such as "Alexa, turn on the lights" and "Ok Google, dim the lights." Renesas' module promises not only quick and easy development but also unparalleled battery life, security features, and compatibility with a wide range of Matter-supported devices, from lighting and thermostats to media devices and beyond. Learn more at Renesas.com/matter.