概要
説明
Embedded Software Applications for Social Distancing Applications
Renesas provides leading-edge software references for distance measurements between Bluetooth® devices. In the COVID-19 pandemic context, this technology can be used for alerting people in keeping a safe social distance to other people. Two different projects are provided as described below.
Accurate measurements based on Renesas' Wireless Ranging (WiRa) technology
WiRa uses a radar-like implementation to greatly enhance distance measurement for connected devices, amounting to +/- 0.5 meters in typical situations. The provided software example runs on the DA1469x family of Bluetooth devices and has been created on top of the SmartBond™ Wireless Ranging SDK.
- Download WiRa SDT SW zip file
- Download Wira SDT HTML document
Distance measurements based on Received Signal Strength Indication (RSSI)
Distance measurements based on RSSI allow for implementation on any Bluetooth-enabled devices. The results are not as accurate as WiRa but it will run on low-end devices and therefore can be created at a lower cost. The provided software example demonstrates the functionality on the DA14531 IC and also on the DA14531 TINY™ Module
ターゲットデバイス
設計・開発
関連ボード&キット
SmartBond™ Wireless Ranging (WiRa™) Software Development Kit
Renesas' Wireless Ranging (WiRa™) Software Development Kit (SDK) enhances the DA1469x family of Bluetooth® Low Energy (LE) System on Chip (SoCs) with highly accurate and reliable distance measurement capabilities. Current market offerings fall short due to the radio signal strength indicator... 続きを読む