概要
The SSC Replacement Board is included in Renesas' modular SSC Evaluation Kits for select resistive sensor signal conditioner (SSC) ICs. It simulates a variable sensor signal for the Evaluation Kit via an on-board potentiometer. It is an option that can be used for a dry-run or demonstration calibration while the user's sensor is in development.
特長
- SSC Replacement Board
サンプル&ご購入
SSCSENSORREPBDV2P0
アクティブ拡張ハードウェア
SSC Communication Board
SSC Mass Calibration Board
SSC Mass Calibration System Power Switch Board
The SSC Mass Calibration System Power Switch Board supports the SSC Mass Calibration Systems for the ZSC31010, ZSC31015, and ZSC31050 sensor signal conditioner (SSC) ICs (DUTs). It enables switching a power supply for the DUTs of up to 40VDC. It is ordered separately.
ZSC31010 Evaluation Kit
ZSC31014 Evaluation Kit
ZSC31015 Evaluation Kit
ZSC31050 Evaluation Kit
ZSC31150 Evaluation Kit
Evaluation Kit for ZSSC313x
The ZSSC313xKIT Evaluation Kit provides the hardware needed for configuration, calibration and evaluation of the ZSSC3131, ZSSC3135, ZSSC3136 and ZSSC3138 Sensor Signal Conditioner (SSC) IC. The user's PC can communicate with the ZSSC313x IC socketed on the ZSSC313x SSC Evaluation Board via the... 続きを読む