Skip to main content
Renesas Electronics Corporation

Renesas Electronics Offers Complete Automotive Integrated Cockpit Reference Solution Based on R-Car System on Chip

Out-of-the-Box Development Experience Shortens Time to Market with Production-Focused Hardware and Software

May 29, 2019

TOKYO, Japan – Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today introduced the Renesas Cockpit Reference Solution, providing an out-of-the-box development experience for quick and cost-effective digital cockpit application design. Developed based on Renesas R-Car M3 system-on-chip (SoC), the Renesas Cockpit Reference Solution delivers a combination of production focused, module-level hardware and software developed by Renesas with additional software from Renesas’ automotive partner network to ease the burden of system-level design.

Image
Figure 1: Example of cockpit display produced by Cockpit Reference Design
Figure 1: Example of cockpit display produced by Cockpit Reference Design

“Automotive integrated cockpit is a challenging space because the integration of so many different cockpit functions, such as multiple operating systems, a rich UI, Bluetooth, and navigation, requires significant system-level insight,” said Daniel Sisco, Senior Director of Automotive Systems, Renesas Electronics. “Leveraging Renesas' deep expertise in both silicon and system-level design, our reference solution reduces the implementation burden, allowing customers to jumpstart their application development in a cost-effective way with production-focused hardware and software.”

Renesas will demonstrate the new Cockpit Reference Solution in Renesas’ booth C190 at TU-Automotive Detroit 2019, June 5-6, in Novi, Mich.

Image
Figure 2: Cockpit Reference Solution Electronic Control Unit (ECU)
Figure 2: Cockpit Reference Solution Electronic Control Unit (ECU)

Key Features of the Renesas Cockpit Reference Solution:

The new reference solution provides OEMs and Tier 1s a full white box baseline solution that can be customized to meet different application requirements. Based on the company’s high-performance R-Car M3 SoC, the cockpit solution is pre-configured to showcase hardware and software features for out-of-the-box development. Customers can then reconfigure, upgrade, or expand on the system to create tailored solutions that match their unique needs.

The solution is delivered as a transparent mixture of FOSS (Free and Open-Source Software), Renesas software and third-party software by key members of Renesas’ automotive partner network. OEMs and production partners can modify, change, and distribute the Renesas code to best fit the application design needs.

The electronic control unit (ECU) reference solution delivers a functional, high-quality baseline implementation for multi-function display cockpit applications. Renesas offers customers a full turn-key, automotive, LPDDR4 (Low power DDR4 memory) reference design to address the challenge of high-speed IO interface design, complete with design and test collateral. Once customers customize the PCB for their own proprietary feature set, the reference design allows them to quickly bypass the traditionally steep learning curve.

Delivered as source code, the software package enables users to jumpstart application design with no existing cockpit solutions or collateral required. The package represents a complete reference cockpit solution, including BSP (board support package) and drivers, operation system (OS), virtualization example, Automotive-Grade Linux example, middleware, and a full application layer.

Availability

The Renesas Cockpit Reference Solution is available now. Please contact your local sales representative for more details. Renesas will continue to update and expand the solution with new software features moving forward, aligning with automotive industry trends.

More Information

To learn more about the new Renesas Cockpit Reference Solution, visit: https://www.renesas.com/solutions/automotive/car-information-system.html

To learn more about Renesas’ R-Car M3 SoCs, visit: https://www.renesas.com/en/solutions/automotive/soc/r-car-m3.html.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.