Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The Linux PTP stack (ptp4l) and clocking devices like ClockMatrix™ now give users the ability to develop non-telecom solutions that are entirely open-sourced. Having a tested, proven solution for either Grand Master or slave clock generation establishes an easy launching point for developers that significantly reduces time-to-market to allow focus on innovative, differentiated, winning solutions.

Renesas Precision Time Protocol (PTP) Clock Manager for Linux (pcm4l) software supports IEEE 1588 and Synchronous Ethernet communication requirements to meet stringent ITU-T Network Synchronization and time distribution. PTP Clock Manager is meant to complement an IEEE 1588-2008/2019 compliant PTP stack and features a clock servo and Packet Delay Variation (PDV) filter to meet the needs of ITU-T standard G.8273.4 and G.8263. While designed for use with the ClockMatrix synchronizers from Renesas, which support ITU-T standard G.8273.2 filtering in hardware, it can also be used with older generation devices. The PTP Clock Manager software is provided free of charge (under license) as long as it is paired with a clock synchronization device (such as the 8A34001) from Renesas.

In conjunction with this software, Renesas has developed and helps maintain a PTP kernel driver in mainline Linux, creating a proven solution for managing timestamps and establishing synchronization across the network. Renesas is actively working with TSU vendors to get the PTP kernel drivers included in their software distribution. We expect customers to have the PTP kernel drivers implemented and functioning properly prior to attempting to use the PTP Clock Manager software. For designs based on AMD Zynq™ UltraScale+™ RFSoC, please refer to the ZCU670 Evaluation Kit and 2024.1 Ethernet TRD. For designs based on AMD Zynq UltraScale+ MPSoC, Renesas can provide a ZCU102 FPGA Mezzanine Card (FMC) and files based on Vivado/PetaLinux 2020.1. If more hands-on assistance is required, customers should engage with sales to discuss fees applicable for such support.

The primary source of the Renesas Clock Synthesizer driver set is from the Linux kernel. Our in-tree drivers can be found in the kernel source under drivers/ptp (for ptp_clockmatrix.c, ptp_clockmatrix.h, ptp_idt82p33.c, and ptp_idt82p33.h) and drivers/mfd (for rsmu, rsmu_i2c, and rsmu_spi). Since there is a delay to get the most recent version of the drivers accepted into the kernel and additional delay for individual distributions to align with the kernel, we also provide a site for customers to get the most recent (out of tree) version of the driver set at renesas/linux-ptp-driver-package (github.com). This site also provides the source for the rsmu drivers which provides additional interfaces used by pcm4l and user software to access the clock synthesizer.

For processing the ESMC (Ethernet Synchronization Messaging Channel) quality level messages and controlling the SyncE DPLL, Renesas provides the Synchronous Ethernet Daemon (synced) software.

Combining the power of the kernel, PTP Clock Manager, and ClockMatrix devices, customers can easily deploy the Renesas solution with any vendor’s Time Stamp Unit (TSU) for their telecom and non-telecom applications. Many TSU vendors also offer kernel drivers in Linux, establishing a plug-and-play development environment.

Demand for synchronization across the internet and throughout global communications networks is increasing. At the same time, the demand for tighter and tighter synchronization is growing, and networks are adapting to support these demands. Operators are also looking to reduce costs and spur innovation by migrating to O-RAN and White Box network solutions. As new vendors enter the fray, the call for open-sourced SW to support the demands of IEEE1588 and Synchronous Ethernet networks is loud. Renesas offers a compelling solution with the first such software – the Precision Time Protocol (PTP) Clock Manager for Linux.

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 837 KB
Software & Tools - Other
Log in to Download ZIP 132 KB
2 items
Type Title Date
Manual - Software PDF 646 KB
Manual - Software PDF 715 KB
Manual - Software
Log in to Download PDF 2.25 MB
Manual - Software
Log in to Download PDF 912 KB
Datasheet PDF 2.11 MB
White Paper PDF 400 KB
Open RAN uses the eCPRI interface to connect radio and distributed units in fronthaul networks, requiring precise timing synchronization. This paper discusses timing accuracy standards and how IEEE 1588 Precision Time Protocol enables synchronization across network elements. It highlights how clock characteristics affect deployment flexibility and cost by influencing the number of telecom boundary clock hops supported. The paper also presents time synchronization hardware and software solutions that meet stringent timing requirements for Open RAN and eCPRI systems.
White Paper PDF 276 KB
This whitepaper reviews the Linux PTP Hardware Clock (PHC) subsystem infrastructure and the uses of the PHC as an interface to both software-based and hardware-based servos that provide the Telecom synchronization interfaces required to meet ITU-T network limits for 5G Radio Access Network (RAN).
Manual - Software PDF 812 KB
White Paper PDF 975 KB
Packet delay variation (PDV) in PTP-unaware networks can cause wander in IEEE 1588 slave clocks, impacting telecom synchronization. This paper compares PDV filtering versus low-pass filtering in servo loops, showing PDV filters achieve up to 60× better performance and meet ITU-T G.8261 limits. Renesas PTP Clock Manager provides PDV filtering and compliance for cost-effective, high-accuracy frequency synchronization.
Application Note PDF 135 KB
AI-generated Summary: ClockMatrix firmware versions 4.8.7 and 5.2.2 support compatibility with the Linux PHC (PTP Hardware Clock) driver. Firmware version details can be checked via specific device registers for major, minor, and hotfix releases. Linux Kernel version 5.11 or later is recommended to use these firmware versions, with backporting options available for earlier kernels. This ensures proper synchronization and timing management using ClockMatrix devices with Linux systems.
Manual - Software PDF 294 KB
White Paper PDF 342 KB
Linux kernel support for IEEE 1588 hardware timestamping enables nanosecond-level synchronization through PHC infrastructure and SO_TIMESTAMPING APIs. These standardized interfaces simplify integration, improve driver availability, and reduce development costs. Renesas ClockMatrix devices and PTP Clock Manager software provide advanced timing solutions for telecom and industrial applications requiring high precision and PDV filtering.
12 items

Support Communities

  1. PTP Clock Manager for Linux ZCU102 reference design availability

    Hello, My group is evaluating the clockmatrix devices for synchronizing our ZynqMP+ devices and would like to use the pcm4l.  The web site says there are reference files for the ZCU102, can someone direct me to those?  I have also requested access to the pcm4l Software, but I've never ...

    Apr 8, 2025
  2. How to build xen + yocto for rcar m3 + kingfisher board.

    ... m3ulcb/build/tmp/work/m3ulcb-poky-linux/xen-image-minimal/1.0-r0/oe-rootfs-reporepo: using cache for: oe-reponot found other for: not found modules for: not found deltainfo for: not found updateinfo for: oe-repo: using metadata from Thu 28 ...

    Oct 29, 2021
  3. Segmentation fault error for Modbus/ Profinet example code

    ... We have followed the process as per quick start guide and generated the .bin file. While running on the RZ/N1D board we are getting the segmentation fault. Also, i have noticed that all the example code are only for RZN1s board. Please help us to resolve the issue.

    Aug 17, 2023
View All Results from Support Communities (52)