Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Migrating between Integrated Development Environments

Renesas offers multiple integrated development environments (IDEs) to help support development. e² studio and CS+ (formerly CubeSuite+) are the most complete development environments we offer, and we offer several other special-purpose IDEs, including PM+ (Project Manager), and the High-performance Embedded Workshop (HEW). If you decide to change development environments, please use the following information to help you migrate your projects and/or code.

Please review the following precautions prior to changing IDEs, compilers, or debuggers.

How to Migrate Between Environments

Differences in Functionality and Operation

Functionality and SettingsSummaryPM+HEWCS+e² studio
Project managementBatch management of files, settings, etc.lenslenslenslens
Changing the MCUChanging the MCU after project creationlenslenslenslens
Rapid BuildSpeeding up the build time——lenslens
Customizing the buildSpecifying make rules applied when building a project—lenspanorama_fish_eye (Note1)lens
Call GraphDisplaying call Graph for functions—panorama_fish_eyelenslens
Function ListDisplaying lists of function addresses, references, etc.——lenslens
Variable ListDisplaying lists of variable addresses, attributes, etc.——lenslens
Detailed setting of eventsEvent setting during debugginglenslenslenslens
Tracking event conditionsTracking event conditions after changing the sourcepanorama_fish_eyepanorama_fish_eyelenslens
Debug SessionsManaging multiple emulators or download settings—lenspanorama_fish_eye (Note2)lens
Action eventsDisplaying values and comments when running a specific portion of the codepanorama_fish_eye (Note3)panorama_fish_eye (Note3)lens (Note3)panorama_fish_eye (Note3)
SettingsBuild options, debug settingspanorama_fish_eyepanorama_fish_eyelenslens
Pack functionSaving and restoring tools used——lens—
UpdatingAutomatic version updating—lenslenslens
Command lineFunction for performing IDE operations by means of commands—lenslenslens

lens Supported, or equivalent functionality is supported | panorama_fish_eye Supported, but relatively inferior | — Unsupported | HEW High-performance Embedded Workshop

Notes

  1. CS+ allows specification of commands only before and after operations such as build, compile, and assemble.
  2. CS+ does not use the concept of sessions, instead allowing a single set of settings for each individual debugging tool. Multiple download file settings are therefore possible. Settings are entered in the properties of the debugging tool.
  3. Equivalent functionality is available by using printf in PM+, High-performance Embedded Workshop, and the e² studio (however, with PM+, this is only available on the simulator, and with the e² studio, this is only available on the virtual console). CS+ can output variables and comments without requiring code specifically for this.

Migrating Between Integrated Development Environments

The documents listed below describe the differences in how projects operate in the different integrated development environments (IDEs). Please review prior to changing IDEs.

HEW

High-performance Embedded Workshop

NC30WA

C/C++ Compiler Package for R8C and M16C Families

H8C

C/C++ Compiler Package for H8SX, H8S, H8 Family

SHC

C/C++ Compiler Package for SuperH Family

RXC

C/C++ Compiler Package for RX Family (IDE: High-performance Embedded Workshop)

CA78K0R, CA78K0

C Compiler Package for RL78 and 78K Families

CX

C Compiler and IDE for V850 Family (for V850E2M core and V850E2S core)

CA850

C Compiler and IDE for V850 Family (for V850E1 core and V850ES core)

Migrating Between Compilers

The documents listed below describe the differences in options or extended language specifications, and describes precautions that must be taken when changing compilers.

NC30WA

C/C++ Compiler Package for R8C and M16C Families

H8C

C/C++ Compiler Package for H8SX, H8S, H8 Family

SHC

C/C++ Compiler Package for SuperH Family

CA78K0R

C Compiler Package for RL78 and 78K Families

CA850

C Compiler and IDE for V850 Family (for V850E1 core and V850ES core)

CX

C Compiler and IDE for V850 Family (for V850E2M core and V850E2S core)

Functions to support porting

Migrating Between Debuggers

The documents listed below describe the differences in debugger operation. Please review prior to changing IDEs.

HEW

High-performance Embedded Workshop