Skip to main content
Renesas Electronics Corporation

Overview

The RX62T Low Voltage Motor Control Evaluation System is only supported for existing customers.

Features

  • This kit is ideal for the following purposes: evaluation of Renesas devices (CPU products, A&P products), evaluation of sample programs provided by Renesas and as a reference when customers design boards and software.
  • A sample program for motor control by the following method is included.
  • 120 degree conduction using Hall sensor*
  • Sensorless 120 degree conduction*
  • Encoder vector 180 De-energizing*
    * Not included in the kit.

Products in the Design

Sample & Buy

RX62T Low Voltage Motor Control Evaluation System

RX62T-Low-Voltage-Motor-Control

Obsolete
ECCN (US):3A991.a.2
HTS (US):8471.50.0150

Videos & Training