Skip to main content
Renesas Electronics Corporation

Description

As a CPU board usable in connection with the on-chip debugging emulator E2, E2 Lite, this product achieves simple and easy evaluation of the target MCU.

Features

  • Incorporates RL78/F24 (R7F124FPJ)
  • 4MHz resonator and 32.768kHz resonator are mounted
  • Equipped with universal area (2.54 mm pitch)
  • Supports both flash memory programming and on-chip debugging (using TOOL0 pin)
  • Highly extendable featuring peripheral board connectors equipped with microcontroller pins

Applications

Type Title Date
Manual - Development Tools
Log in to Download PDF 519 KB
Application Note PDF 813 KB 日本語
This application note describes how to write the program to the internal flash memory of the RL78 MCUs that supports the RL78 Protocol D by the Raspberry Pi 4 Model B+. Serial programming of the RL78 Protocol D is used for writing. The Raspberry Pi is used as a programmer; the program rewriting file is executed to send the rewrite data for the write operation.
Application Note PDF 1.69 MB 日本語
This application note describes how to write the program to the internal flash memory of the RL78 MCUs that supports the RL78 Protocol D. Serial programming of the RL78 Protocol D is used for writing. There are two modes: Online Mode, in which the host PC sends commands to perform rewriting, and Offline Mode, in which the data to be rewritten is downloaded from the host PC in advance and rewriting is triggered by pressing a switch.
Application Note PDF 456 KB
AI-generated Summary: The CAN driver for RL78/F24 supports CAN-FD communication with a single-channel RS-CANFDLite controller. It integrates with the IAR development environment and Renesas E2 debugger for debugging and self-test operations. Hardware requirements include using the RL78/F24 controller with a 20 MHz external quartz or PLL for clock accuracy, a 5V power supply, and proper jumper and CAN bus termination settings. The software architecture includes SmartConfigurator-generated drivers, upper driver APIs, and monitor programs for interactive CAN self-tests. The package includes configuration files, source code, and project files compatible with IAR EW 5.10.1 or higher. The document references detailed manuals and tools for setup and debugging.
4 items

Software & Tools

Software & Tools

Software title
Software type
Company
E2 emulator [RTE0T00020KCE00000R]
On-chip debugging emulator. Also available as a flash memory programmer. [Support MCU/MPU: RA, RE, RH850, R-Car D1, RL78, RX, RISC-V MCU]
Emulator Renesas
E2 emulator Lite [RTE0T0002LKCE00000R]
On-chip debugging emulator. Also available as a flash memory programmer. [Support MCU/MPU: RA, RE, RL78, RX, RISC-V MCU]
Emulator Renesas
2 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 1.89 MB 日本語 Function: Application Example
This application note describes how to write the program to the internal flash memory of the RL78 MCUs that supports the RL78 Protocol D by the Raspberry Pi 4 Model B+. Serial programming of the RL78 Protocol D is used for writing. The Raspberry Pi is used as a programmer; the program rewriting file is executed to send the rewrite data for the write operation.
Sample Code
Log in to Download ZIP 35.25 MB 日本語 Function: Application Example
This application note describes how to write the program to the internal flash memory of the RL78 MCUs that supports the RL78 Protocol D. Serial programming of the RL78 Protocol D is used for writing. There are two modes: Online Mode, in which the host PC sends commands to perform rewriting, and Offline Mode, in which the data to be rewritten is downloaded from the host PC in advance and rewriting is triggered by pressing a switch.
Sample Code
Log in to Download ZIP 255 KB
Application: Automotive
Function: CAN IDE: IAR EWRL78
Sample Code ZIP 22 KB
4 items
Part NumberStatusStockBudgetary Price (USD)SampleablePb (Lead) FreeECCN (US)HTS (US)RoHS CompliantChina RoHS Compliant
RTK7F124FPC01000BJActiveIn Stock1u | $82.35AvailableNo3A991.a.28471.50.0150NoNo

Support Communities

  1. Troubleshooting Communication Issues Between E2 Lite Debugger and RL78/F24 Target Board After Renesas Flash Programmer (RFP) Programming

    First_Project.zip I am currently using the RL78/F24 target board RTK7F124FPC01000BJ and E2 Lite for development.I previously developed and executed a simple LED blinking example in e2studio (code below), and after debugging, the functionality was normal.I could see the LED on the TARGET BOARD blinking ...

    Apr 24, 2025
  2. RL78/F24 example software demo code

    RL78/F24 可以提供GPIO, UART, I2C, UART, ADC 等 驱动程序学习?我正在调试是用RTK7F124FPC01000BJ demo baord,但在官网没有找到相关demo code.

    Apr 19, 2024
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
Icon showing CD-ROM illustration, indicating compact disc storage.

ROM Ordering

Embed your custom code into Renesas masked MCUs during manufacturing for tailored device functionality.