Overview
Description
The EK-RA8D1 evaluation kit enables users to effortlessly evaluate the features of the RA8D1 MCU Group and develop embedded systems applications using Renesas' Flexible Software Package (FSP) and e2 studio IDE. Utilize rich onboard features along with your choice of popular ecosystem add-ons to bring your big ideas to life.
The EK-RA8D1 kit consists of three boards: the EK-RA8D1 board featuring the RA8D1 MCU with on-chip graphics LCD controller, a MIPI graphics expansion board featuring a 4.5-inch TFT color LCD (480 x 854) with capacitive touch overlay, and a camera expansion board featuring a 3M pixels CMOS image sensor.
Getting Started
Running the Quick Start Example Project
- The EK-RA8D1 board comes pre-programmed with a quick start example project (source code provided in the EK-RA8D1 example project bundle).
- Connect the MIPI graphics and camera expansion boards to the MIPI graphics (J58) and camera (J59) expansion ports on the EK-RA8D1 board.
- Power up the EK-RA8D1 board through the USB debug port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
- The quick start example project will begin to execute showing the graphic elements on the screen.
- Refer to the EK-RA8D1 Quick Start Guide to explore additional functionality of the quick start example project.
Developing Embedded Applications
- Modifying the Quick Start example project – refer to the EK-RA8D1 Quick Start Guide for instructions on importing, modifying, and building the quick start example project.
- Start with one of the many other example projects (provided in the EK-RA8D1 example project's bundle) – choose from many example projects to learn about different peripherals of the RA8D1 MCU group. These example projects can serve as excellent starting points for you to develop your custom applications.
Building Custom Hardware
- Start by building a functional prototype - utilize the EK-RA8D1 board with your choice of ecosystem add-ons.
- Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA8D1v1 Design Package.
Features
- Special Feature Access:
- MIPI DSI and Parallel Graphics Expansion Ports
- Camera Expansion Port
- Ethernet
- USB High-Speed Host and Device
- 64MB SDRAM
- 64MB External Octo-SPI Flash
- MCU Native Pin Access:
- R7FA8D1BHECBD MCU
- 480MHz, Arm® Cortex®-M85 core
- 2MB Code Flash, 1MB SRAM
- 224 pins, BGA package, 13mm x 13mm x 1.47mm, 0.8mm pitch
- Native pin access
- MCU and USB current measurement
- DC/DC mode configuration
- Ecosystem and System Control Access:
- USB Full Speed Host and Device
- Multiple 5V input sources:
- USB (debug, full speed, high speed)
- External power supply
- SEGGER J-Link™ onboard programmer and debugger
- Debug modes:
- Debug onboard (SWD) – via J-Link
- Debug out (SWD) – via J-Link
- Debug in (ETM, SWD and JTAG) – via J-Link, Arm® Keil® ULINK™, IAR I-jet™, Renesas E2/E2 Lite, etc.
- User LEDs and buttons:
- Three user LEDs (red, blue, green)
- Power LED (white) indicating the availability of regulated power
- Debug LED (yellow) indicating the debug connection
- Two user buttons
- One reset button
- Five most popular ecosystem expansions:
- MikroElektronika™ mikroBUS connector
- SparkFun® Qwiic® connectors (may not be populated)
- Two SeeedGrove® system (I2C and analog) connectors (may not be populated)
- Two Digilent Pmod™ (SPI and UART) connectors
- Arduino® (UNO R3) connector
- MCU boot configuration
- MIPI Graphics Expansion Board:
- 4.5 Inch backlit TFT display, 16.7M display colors
- 480x854 pixels resolution
- 2-lane MIPI interface
- Capacitive touch overlay (I2C)
- Camera Expansion Board:
- Off-the-shelf Arducam CMOS OV3640 Camera Module
- ¼ Inch 3.1 Megapixel image sensor
- Up to 15 fps in QXGA (2048x1536 pixels) resolution
Applications
Design & Development
Videos & Training
This tutorial demonstrates how to build a PTX NFC basic application from scratch by adding the required software stacks on the RA8D1 Evaluation Kit. The example project uses the RA8D1 Evaluation Kit together with the PTX105R NFC controller board to showcase IoT functionality and integration.
Additional Videos
News & Blog Posts
News Dec 12, 2023 |
Blog Post Dec 12, 2023 |
Blog Post Jan 28, 2022 |
Blog Post Jan 28, 2022 |
Blog Post Nov 18, 2021 |
Blog Post Nov 11, 2021 |
Certifications
The EK-RA8D1 kit meets the following certifications/standards. Refer to the EK-RA8D1 user manual for the disclaimer, precautions and more details on the certifications.
EMC/EMI Standards
- FCC Notice (Class A) – Part 15
- Innovation, Science and Economic Development Canada ICES-003 Compliance: CAN ICES-3 (A)/NMB-3(A)
- CE Class A (EMC Directive 2004/108/EEC)
- Taiwan Chinese National Standard 13438, C6357 compliance, Class A limits
- Australia/New Zealand AS/NZS CISPR 32:2015, Class A
Material Selection, Waste, Recycling, and Disposal Standards
- EU RoHS
- China SJ/T 113642014, 10-year environmental protection use period
Safety Standards
- UL 94V-0
Support
Support Communities
- quickstart_ek_ra8d1_ep_examples Not Building
I have tried building the QuickStart program given for ek-ra8d1 given in EK-RA8D1 Example Project Bundle, but I am getting multiple errors. I am attaching the build log for your reference. Please provide needful assistance. 2047.log.txt
Mar 14, 2024 - Build error on FileX_exFAT_block_media_sdmmc_ek_ra8d1_ep example
Dear all, I am facing this building error on the FileX_exFAT_block_media_sdmmc example project. "No rule to make target '../ra/microsoft/azure-rtos/threadx/common/src/tx_block_pool_initialize.c' " The example has been retrieved from r20an0717eu0105-ek-ra8d1 ...
Apr 9, 2024 - LVGL in EK-RA8D1
EK-RA8D1 with LVGL example project
Aug 28, 2024
Knowledge Base
- RA and FSP Curriculum : Getting Started with EK-RA8D1 Graphics Application Embedded Wizard
Last Updated: 30 Oct 2024 This lab material explains all necessary steps to create an Embedded Wizard UI application suitable for RA8D1 Evaluation Kit. Getting Started with EK-RA8D1 Graphics Application Embedded Wizard for FSP 5.5.0 - a hands on lab using EK-RA8D1, Embedded Wizard Studio and FSP ...
Oct 30, 2024 - RA Family: Note on xSPI memory programming using FSP OSPI Write API
... amount of data that can be written in one command is restricted by this page size. For example, the S28HL512T OSPI memory used on the EK-RA8D1 supports a page size of 256 bytes or 512 bytes. Please refer to the memory device user's manual for more details. Size ...
Jul 10, 2025 - RA Family: How to adjust touch panel input coordinates when display orientation is changed
When the screen is rotated, the touch panel coordinates also need to be converted accordingly. Using the following application note for the EK-RA8D1 as an example: Develop Graphics Applications Using the MIPI DSI Interface on the RA8D1 (R01AN7362) As shown above, for Clockwise (90), add the following settings for ...
Apr 28, 2025