Skip to main content
Renesas Electronics Corporation

Overview

The DA14530 SmartBond TINY™ Development Kit Pro (DA14530-00FXDEVKT-P) is the most ideal way to quickly and easily get started developing applications and products using the DA14530 Bluetooth® Low Energy (LE) system-on-chip (SoC).

The DA14530-00FXDB-P is the FCGQFN24 daughterboard for the DA14530 Development Kit Pro's motherboard.

Products in the Design

Sample & Buy

DA14530 Daughter Board

DA14530-00FXDB-P

Active
MOQ:1
SPQ:1
Pb (Lead) Free:Yes
Carrier Type:Box
Assembly Location:GERMANY
1u | $14.00Budgetary Price

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

SmartBond TINY DA14530 Bluetooth Low Energy 5.1 System-on-Chip Development Kit Pro

Develop and evaluate Bluetooth Low Energy applications using the DA14530 SmartBond TINY platform. The kit supports rapid prototyping of compact, low-power wireless designs.