Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

RZ/G2 64-bit MPUs Overview

RZ/G2 64-bit MPUs Overview
Feb 21, 2019

About This Video

Renesas introduces the second generation RZ/G series of 64-bit microprocessors (MPU) with verified Linux package. The RZ/G2 MPUs offer high performance, high reliability embedded microprocessors with advanced graphics for next generation Human-Machine Interfaces (HMI) on industrial and building automation systems.