Skip to main content
Renesas Electronics Corporation

Renesas’ New GaN Charging Solution Delivers 500W of Power to Wide Range of Industrial and IoT Electronics

GaN-Based HWLLC Converter Topology Sets New Power Density and Peak Efficiency Benchmarks for Next-Generation Computing Devices, Power Tools and e-Bikes, basic_html

March 23, 2026

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, has expanded its suite of AC/DC and power adapter solutions with a new GaN-based Half-Wave LLC (HWLLC) platform that supports 500W or higher operation across IoT, industrial and infrastructure systems. The new HWLLC converter topology scales an ultra-efficient, compact power architecture from 100W-class designs to 500W, enabling the next wave of high-speed chargers for power tools, e-bikes and other appliances without the size, heat and efficiency penalties of legacy topologies.

The portfolio expansion adds four controller ICs that build on Renesas’ proprietary zero-standby power (ZSP) technology. At the heart is the RRW11011, an interleaved power factor correction (PFC) and HWLLC combo controller engineered for high power density and high efficiency. The PFC with phase-shift control cancels ripple, reduces component size and cost, balances current and ensures robustness. The combo controller allows designers to lower operating temperature while delivering the wide output range (5V to 48V) required by USB Extended Power Range (EPR) and other variable-load charging systems. The new solution also features the RRW30120 USB Power Delivery (USB PD) protocol and closed-loop controller, which achieves maximum USB power delivery of 240W, and the RRW40120 half-bridge GaN gate driver and RRW43110 intelligent synchronous rectifier controller. Together in a 240W USB EPR power adapter design, the new solution achieves the highest power density in the industry (3W/cc) and 96.5 percent peak efficiency.

The HWLLC’s wide 500W power envelope broadens the addressable charging market to encompass large TVs and monitors, as well as higher-power appliances like vacuums, power tools, outdoor and industrial lighting and some medical devices. The new HWLLC-based AC/DC topology also helps designers move beyond 100W USB-C charging devices and adopt 240W USB EPR charging to shrink proprietary brick chargers in smartphones, laptops and many gaming systems. Renesas’ compact, high-power fast charging technology was recently incorporated into a GaN-based charger from Belkin. The Belkin Z-Charger features an innovative ZSP chip with Renesas’ advanced SuperGaN® depletion mode (d-mode) GaN technology.

“The Belkin Z-Charger is a major step toward a new era of ultra-low standby power consumption in fast charging,” said Jenny Ng, General Manager of Belkin Asia.

GaN Proves Essential for Increasing Efficiency and Power Density

GaN technology drives the efficiency and power density behind Renesas’ next-generation AC/DC designs, enabling higher switching performance that helps shrink magnetics, reduce losses and keep thermals in check. Renesas’ SuperGaN d-mode technology employs a cascode configuration that is more robust and easier to drive than other GaN implementations, with a higher threshold voltage and drop-in compatibility with standard silicon gate drivers. The result is a faster path for customers to achieve compact, high-efficiency power supplies they can scale, validate and manufacture with greater confidence.

“Renesas’ HWLLC ecosystem brings interleaved PFC and resonant power conversion into a single, harmonized solution that delivers ultra-compact, wide-range AC/DC power with proven efficiency, low standby consumption and trusted integration support,” said Rohan Samsi, Vice President, GaN Business Division at Renesas. “By strategically developing four advanced controller ICs, we’ve created the most optimized, coordinated ecosystem where each element contributes to higher density, improved thermals, reduced EMI/noise and greater operating efficiency.”

By eliminating transformer winding and reducing component count versus traditional LLC implementations, Renesas reduces design complexity and enables more compact magnetics. The enhancement accelerates design re-use across product families that support different wattages, voltages and form-factors while improving reliability and easing BOM management. The highly integrated, wide Vin/Vout offline solution helps customers build smaller, cooler and readily compliant products while achieving standout no-load/standby performance that supports higher energy-efficiency ratings.

Renesas will showcase the HWLLC solution in booth #1219 at the Applied Power Electronics Conference (APEC), in San Antonio, Texas, March 22-25, 2026.

Availability

The four new devices enabling the HWLLC solution are available today in addition to an evaluation board. The EBC10293 240W USB PD EPR Evaluation Board includes integrated PFC, high-efficiency AC/DC conversion and USB PD control in a compact, high-power density design.

Winning Combinations

Renesas offers 240W AC/DC Adapter and 300W Lighting Power Platform solutions that combine the new products with numerous compatible devices from its portfolio. These Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly. They can be found at renesas.com/win.

Get Powered by Renesas

Driven by innovation, quality and reliability, Renesas leads the way in power electronics, shipping more than four billion parts per year from our portfolio of power management ICs, discrete and wide-bandgap GaN products, computing power devices and many more. These products span all major segments including automotive, IoT, infrastructure and industrial applications. Our power portfolio seamlessly attaches to our leading MCU, MPU, SoC and analog solutions, simplifying and accelerating the design process with hundreds of engineering-vetted Winning Combinations and innovative tools such as PowerCompass™ and PowerNavigator™ design software. Find out more at renesas.com/power.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.