Skip to main content
Renesas Electronics Corporation

Overview

DA14580PRODTLKT is not recommended for new designs. The recommended alternative is the Connectivity Production Line Tool.

Renesas offers a production test and programming unit that enables you to reduce the time to ramp-up at a lower cost. The SmartBond Production Line Tool (PLT) helps to increase throughput in volume test and programming of units centered around the Renesas Bluetooth® ICs.

We work with a number of 3rd parties and distributors globally to support this platform. Contact your local Renesas sales office if you would like more information on how Renesas can support your volume production test and programming.

The release of the SmartBond Production Line Tool supports devices in the SmartBond™ Bluetooth families: DA1453x, DA1459x, DA1469x, and DA1470x.

Features

  • Ease of integration: DLL based commands
  • Flexibility in programming OTP/Flash/EEPROM
  • Low overall cost of tester equipment
  • High level of parallelization and short testing time
  • Up to 16 times parallel programming and test

Sample & Buy

DA14580PRODTLKT Production Line Tool Kit Board

DA14580PRODTLKT

Not Recommended for New Designs
MOQ:1
SPQ:1
Pb (Lead) Free:Yes
Carrier Type:Box
Assembly Location:GERMANY
1u | $1,100.00Budgetary Price

Support

Support Communities

  1. Issue with E2 Lite Debugger Not Appearing in e² studio

    Good Morning, I am experiencing an issue with my E2 Lite debugger while using e² studio. The debugger is not appearing as an option in the Debug Hardware selection—only J-Link is available. I have tried the following troubleshooting steps without success: Verified that E2 Lite is properly connected ...

    Mar 26, 2025
  2. DA14531 for mass production programming

    Hello team renesas, I want to know the process of programming DA14531 in mass production. Here we want to store our firmware in SPI flash not in OTP so we can preform SUOTA. So how can i perform this and also guide what changes should i do in firmware before ...

    Nov 21, 2022
  3. DA14680 J-Flash configuration missing

    Hi Folks, we have to bringup a rather old project in which a DA14680 is used. According to the documentation, the recommendation to flash the device is by using the SEGGER J-Link / J-Flash toolchain (is this correct?). Using J-Flash the DA14680 could be selected, but there ...

    May 11, 2023
View All Results from Support Communities (23)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?