QE for Capacitive Touch: Development Assistance Tool for Capacitive Touch Sensors

Overview

This development assistance tool supports the development of embedded systems which use the capacitive touch sensors. It supports MCUs of the RX and the RA families.

Topics

New release: QE for Capacitive Touch[RA] V1.0.0
This tool simplifies the development of RA-family-based systems that work with touch sensors.

Learn More (Tool News) >>

Release Information

Product Name Latest Ver. Released Target Device Details of upgrade Download Operating Environment
QE for Capacitive Touch[RA] V1.0.0 Oct 08, 2019 RA Family See Tool News  Download e² studio V7.6.0 or later
QE for Capacitive Touch V1.1.0 Jul 22, 2019 RX Family See Tool News  Download e² studio V7.4.0 or later

Note: For detailed support devices, refer to "Target Devices" below.

Features

QE for Capacitive Touch is an assistance tool for applications which operate under the e² studio integrated development environment.

For the development of embedded systems that are work with capacitive touch sensors, this tool simplifies the initial settings of the touch user interface and the tuning of the sensitivity, thus shortening developing times.

Functions

The GUI makes it easy for even a beginner to develop touch user interfaces.

Simple GUI operations allow even a beginner to create the configuration for use with a touch user interface, monitor the state of input through the touch sensors, and adjust parameters.

Furthermore, since this tool can adjust tuning parameters and reflect the results through display in real-time, it is very useful for finding the appropriate parameters in various situations, such as in the presence of much static electricity or in cases of use with wet hands.

Automatic tuning for touch sensor sensitivity

This tool enables automatic tuning for the sensitivity of the capacitive touch sensors. You can complete basic tuning within a few minutes by following the instructions in the pop-up messages.

Supported Middleware

Device Driver Version
RA Family CSTU (Capacitive Touch Sensing Unit) Driver
Flexible Software Package (FSP) Component for RA Family
Component name: r_ctsu
V0.80
Touch Driver
Flexible Software Package (FSP) Component for RA Family
Component name: rm_touch
V0.80
RX Family Driver for capacitive touch sensor unit
RX Family QE CTSU Module Using Firmware Integration Technology
Module name: r_ctsu_qe
V1.00
Middleware for touch sensors
RX Family QE Touch Module Using Firmware Integration Technology
Module name: r_touch_qe
V1.00

Target Devices

Family Group
RA Family Only those devices of the RA family that have touch sensor functionality are supported.
RA2A1, RA4M1, RA6M1, RA6M2, RA6M3
RX Family Only those devices of the RX family that have touch sensor functionality are supported.
RX113, RX130, RX230, RX231

Information supporting development tools

Title Description
My Renesas Create a My Renesas account to use our tool download services, receive e-newsletter/update notifications, and take advantage of our other services.
e-learning Information for studying and learning about microcontrollers and microprocessors.
FAQ Frequently asked questions and useful hints for development.
Forum A forum and community site to share technical information, questions and opinions with others who use Renesas MCU's.
Tool News Tool release information and other important information.
Operating Environment Information on system requirements and operating environment for the latest version of tools.
Info on Discontinued Products A list of Renesas software and tools that have been discontinued and are no longer being offered for new projects.

Adding and Setting Middleware Related to QE for Capacitive Touch

RA Family: Capacitive touch sensor Pins and Stacks Configuration can be easily performed in conjunction with the Configurator

The following FSP components for RA family are supported.

  • CTSU (Capacitive Touch Sensing Unit) Driver "r_ctsu"
  • Touch Driver "rm_touch"

Add the FSP components related to the Capacitive Touch Sensor and generate project content for the RA family MCU that has the Capacitive Touch Sensor function. Then, run the pins configuration function. In this mode, you can easily set up stack configuration (such as pin assignment for use with capacitive touch sensor pins or Hardware Abstraction Layer (HAL)).

See here for details of Flexible Software Package (FSP) >>

RX Family: Interlinking with the Smart Configurator eases setting up the pins for use with capacitive touch sensors.

When generating a project to which the FIT module related to capacitive touch sensors is to be added, select the checkbox of "Smart Configurator" to run the Smart Configurator. This makes it easy to configure the settings of pin allocation for use with a capacitive touch sensor from the e² studio.

Learn More About QE for Capacitive Touch! Abundant Documents and Usage Guidance

All documents also can be found by clicking on the [Documents] tab on this page.

What can QE for Capacitive Touch help me do?
Tool News (QE for Capacitive Touch)
How do I install QE for Capacitive Touch?
Release Note (QE for Capacitive Touch)
How do I use QE for Capacitive Touch in development?
Application Note: RX Family Using QE and FIT to Develop Capacitive Touch Applications
What are the details of the capacitive touch sensor related FIT module?
Application Note: RX Family QE CTSU Module Using Firmware Integration Technology
Application Note: RX Family QE Touch Module Using Firmware Integration Technology
I need some sample code.
Application Note/Sample Code: RX130 Group RX Capacitive Touch Evaluation System Sample Code for QE Project

How to Find the Version Number

From the [Help] menu of the e² studio, select the [e² studio Installation details] menu item then the [Installed Software] tab to see which version of the "Renesas QE for Capacitive Touch" you have.